Hi Community, I'm Eugenio Mercol from Argentina.
I'm designing an RF detector, using LTC5505 device, manufactured by Analogic Device Company.
Short project description and trouble.
It´s a device that can detect RF signal present in the air, once the signal is detected, and the RSSI value exceed a defined value, the device generate a vibratoring advising, sonoric advising an luminic advising.
This device will be carried by the people like a wereable device, and will be carried all the time.
I´m stucked in the antenna design.
I already download the AN91445 Antenna Design and RF Layout Guidelines.pdf document, (that is a really very good document, Thanks to Tapan Pattnayak!!) but I can't see how calculate the MIFA or IFA length for the frecuencies beetwen 300 to 450 Mhz.
Project Details.
PCB type and Size: two sides, 30mm x 35mm (keychain type)
Device Size: 30mm, x 45mm
Kind of components used: SMD
Power Source: Alkaline 12V A23S cell
Operation Voltage: 3V
Space defined for the antenna in the PCB: 13mm x 22mm.
Range of detection needed: up to 20 meters
Frecuencies detected: beetwen 300 to 450 Mhz
Only for RF reception
Never will be an RF transmisor.
It will be carried by the people, inside the pants pocket.
Questions
1* - Based in the description about, antenna space available, place where the device will be carried by the persons, frequency range, and sensibility needed for up to 20 meters detection. What kind of antenna do you recommend to me, MIFA or IFA?
2* - Depending the kind of the anntena selected. How Can I calculate the length of the antenna?
Thank you very much!
Which Cypress device are you using in conjunction with the RF Detector as this is a support community for Cypress products?
I'm using the CY8C4013SXI-410 microprocessor.
The microprocessor will be in charge to check the RSSI level signal, provided from the LTC5505 device.
Also is voltage battery level checker.
If in some case that the unusual event is present, like battery low level o high RF signal level, the microprocesor will turn the advises on
Thanks eugeniomercol_4116346
I moved this over to the PSoC 4 community so that someone from our applications team can take a look.
Dear eugeniomercol_4116346,
I believe that the questions you have are more related to the Analog Devices device and hence would ask you to seek support from them.
We would be happy to help if you have any queries related to the PSoC device
Regards
Jeet