Hello! I am using a CY8C4A45PVI analog coprossesor and I am trying to put a Switched capacitor filter on my design in PSoC Creator 4.4 , but I have this error: 'Error: fit.M0050: The fitter aborted due to errors, please address all errors and rebuild. (App=cydsfit)'.
I was looking for a solution in the forum and I found that this component works on PSoC Creator 4.2. So, I installed that version, but when I look for the device, the CY8C4A45PVI is not there. Also, I can't find any PSoC 4 with Analog Blocks in that list.
How can I design a Switched capacitor filter in the CY8C4A45PVI Analog coprocessor?
Attached examples of the web that do not work in PSoC creator 4.4
Solved! Go to Solution.
In the top line of Creator, go to Tools, then Find New Devices.
If that doesn't work, contact me directly, dennis.seguine@infineon.com and I'll get more help
from the software guys.
---- Dennis
Hi,
While using Creator 4.4 for these devices the errors are expected.
Problem:
When using a device with a UAB (CY8C4A45PVI-481, CY8C4A45FNI-483, CY8C4A45LQI-483, CY8C4A45AZI-483, CY8C4A25LQI-483, CY8C4A45FNQ-483, CY8C4A45LQQ-483, CY8C4125PVI-PS421, CY8C4125FNI-PS423, CY8C4125LQI-PS423, CY8C4125AZI-PS423, CY8C4145PVI-PS421, CY8C4145FNI-PS423, CY8C4145LQI-PS423, CY8C4145AZI-PS423, CY8C4145PVI-PS431, CY8C4145FNI-PS433, CY8C4145LQI-PS433, CY8C4145AZI-PS433, CY8C4145FNQ-PS423, CY8C4145FNQ-PS433), you may get the error message "System.Collections.Generic.KeyNotFoundException".
Workaround:
The only solution is to use PSoC Creator 4.2.
Additionally the cod example document states that it needs to be used with 4.2 version of the creator.
Now to solve the error you are facing kindly update the component in the project using the following step.
With the latest component you should be able to build the project without any problem.
Best Regards,
Vasanth
Hi Vasanth, thank you for your answer.
I tried to open the project on PSoC Creator 4.2, but I can't select the device CY8C4A45PVI because it doesn't appear on "Select Device" list. How come you have it on your menu and I don't? Is there any way to update the devices on PSoC 4.2?
Best Regards,
Delfina
In the top line of Creator, go to Tools, then Find New Devices.
If that doesn't work, contact me directly, dennis.seguine@infineon.com and I'll get more help
from the software guys.
---- Dennis
It worked! Thank you very much!