- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dear Receiver,
I use built-in example code ( CE210291_CapSense_P4_One_Button02 ) in the PSoC Creator 4.4.
I didn't modified anything but I met a compiler error as shown in the attached file.
What's the meaning of modulation clock ?!
I re-config this parameter to 12000kHz and compiler ok.
Why default setting (24000kHz) is wrong ?!
Thank you so much.
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I downloaded that CE and observed the same error.
Then I skimmed the datasheet of the CapSense component,
and there was the following description.
PSoC 4100/PSoC 4200: 2400 kHz or HFCLK/2, which ever is lower.
And in this case HFCLK is 24MHz, so the HFCLK/2 is 12MHz and lower.
moto
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I downloaded that CE and observed the same error.
Then I skimmed the datasheet of the CapSense component,
and there was the following description.
PSoC 4100/PSoC 4200: 2400 kHz or HFCLK/2, which ever is lower.
And in this case HFCLK is 24MHz, so the HFCLK/2 is 12MHz and lower.
moto