Announcements

Equip yourself to optimize PSoc4 MCUs for Evs at the EV Webinar. Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

KeTa_1341526
Level 5
Level 5
10 solutions authored 5 solutions authored 100 replies posted

Hello,

I am using the MTK tool in the following community and confirm.

Re: HCI commands to measure packet error rates and RSSI

It is possible to execute slide50 [CYBLE MTK Quick Demo Instructions] under the configuration of [MTK option 1 – UART based testing].

I also want to check [MTK Option 2-BLE link based testing] as well.

However, when I try slide14 [MTK Configuration-BLE link based testing], I get a build error in PSoC Creator.

Please tell me how to deal with it.

[environment]

PSoC Creator version: 4.2

Target Device: CY8C4247LQI-BL483 (CY8CKIT-142)

  MTK HOST: CY8CKIT-042-BLE

  MTK DUT  : CY8CKIT-042-BLE

We changed the PRoC type name to the PSoC 4 BLE type name, and are also performing Component Update.

Best regards,

Kenji Takahashi

0 Likes
1 Solution

Hi,

Please set the L2CAP MTU size set in the BLE component to 100 or above as shown in the image and check once.

Thanks

Ganesh

View solution in original post

0 Likes
4 Replies
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi Kenji Takahashi,

Please find the modified file attached with this project which solves this issue. Please replace it in your project.

Thanks and regards

Ganesh

0 Likes

Hi Ganesh,

Build error has been improved.

However, the LED on the MTK host board does not light up like [MTK Host LED indications] on slide 14.

Also, the first test in MTK tool will fail.

pastedImage_0.png

It seems that the DUT can not be found.

It is as follows in CyBLE_MTK.h of MTK project.

#define CYBLE_TESTS_ENABLED 0

Should this be set to 1?

I changed it to 1 and tried build, but an error occurs in Build.

Best regards,

Kenji Takahashi

0 Likes

Hi,

Please set the L2CAP MTU size set in the BLE component to 100 or above as shown in the image and check once.

Thanks

Ganesh

0 Likes

Hi Ganesh,

Thank you for your reply.

By changing the L2CAP MTU Size, I was able to test with MTK Tool.

Best regards,

Kenji Takahashi

0 Likes