- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I have a design with PSOC 4200 BLE device but I am not using any of the bluetooth functionality. I am looking for some guidance on what to do with the unused Bluetooth related pins.
Is it best to leave the antenna open or connected to ground?
Does VDDR need power?
I am using the internal oscillator. Does a 24MHz External Crystal Oscillator (ECO) still need to be connected if the radio is not used? Is it ok to leave these pins open or connect to ground?
Thanks.
Solved! Go to Solution.
- Labels:
-
PSoC general
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
1. If RF pin is not used, then please put a 50 ohm shunt on the Antenna pin. Put the shunt resistance on Antenna pin to GND.
2. If BLE is not used, then power supply is not required to VDDR.
3. External crystal Oscillator(ECO) is not required if BLE is not used. You can disable the ECO from the Clocks tab and ECO pins can be left open.
Thanks,
P Yugandhar.