- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I am having an issue with an attempt to get 3-Wire SPI working. First the vitals:
uC: CYBC4247LQI-BL483
IDE: PSoC Creator v4.0 Update 1 (4.0.0.432)
SPI Component: SPIM_1 created with the SPI Master Bidirecional mode Macro (v 2.50)
Device being communicated with: STMicro LSM303C (Datasheet)
Issue:
After I use SPIM_1_TxDisable() to disable the SPI output from the PSoC device sdat line, I then call a dummy write to generate the required clock cycles to cause the slave device to shift its information out of its registers while also maintaining the CS line low. What I am finding when I watch the signal buss with a logic analyzer is that the dummy write that I do is actually not just generating a dummy value, but seems to be being sent to the RX buffer when I call SPIM_1_ReadRxData() to pull the returned data out of the read buffer it actually seems to be pulling the value from 2 previous reads (still, though being the dummy value).
I have checked this with two different logic analyzers to confirm what is going on. When I use the logic analyzer I see that actually the value that is being transmitted back appears to be just a repeat of what ever the dummy write byte is. For tracking purposes, I am using just a repeat of the register value that I was trying to read. So on the logic analyzer, I am getting a straight 1 for 1 correlation to the register that I am trying to read being pinged back to me as the "read" value, but when I am using the debugging register view, I see that what I pull from the register as the read value was the register of the slave device that I was trying to read two reads ago.
In trying to solve this, I though that perhaps in the 4 byte min sided buffer that some values were behaving strangely, so I call both SPIM_1_ClearRxBuffer() and SPIM_1_ClearFIFO(). These did not change the behavior of what was happening. I currently cannot upload the entire project, but I will see if I can extract the key parts into a new project and then upload it. I have inserted some of the code that I am using that is causing the issue as well as a screen shot of the logic analyzer capture.
I have also uploaded screen shots of the SPIM component configuration for clarity till I can break this out into a separate project that I can upload.
for(;;)
{
AccelRead();
CyDelay(1);
}
uint8_t ReadSPI(uint8_t regValue)
{
uint8_t returnVal;
SPIM_1_ClearRxBuffer();
SPIM_1_ClearTxBuffer();
SPIM_1_TxEnable();
SPIM_1_WriteTxData((regValue | 0b10000000));
//Begin the read process by disabling the Transmit, but write dummy value to cycle the clock
SPIM_1_TxDisable();
SPIM_1_ClearRxBuffer();
SPIM_1_ClearFIFO();
SPIM_1_WriteTxData((regValue | 0b10000000));
returnVal = SPIM_1_ReadRxData();
SPIM_1_TxEnable();
return returnVal;
}
double AccelRead(void)
{
volatile int16_t valueX;
volatile int16_t valueY;
volatile int16_t valueZ;
volatile double magnitude;
volatile uint8_t whoAmI;
//TODO Need to add register information and function definitions
valueX = ReadSPI(0x28);
CyDelay(1);
valueX = valueX << 8 | ReadSPI(0x29);
CyDelay(1);
valueY = ReadSPI(0x2A);
CyDelay(1);
valueY = valueY << 8 | ReadSPI(0x2B);
CyDelay(1);
valueZ = ReadSPI(0x2C);
CyDelay(1);
valueZ = valueZ << 8 | ReadSPI(0x2D);
CyDelay(1);
whoAmI = ReadSPI(0b00001111);
magnitude = sqrt(valueX * valueX + valueY * valueY + valueZ * valueZ);
return 0;
}
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I ran into a similar issue when setting up the SPI component to communicate with a Microchip SPI device; I ran into the issue where the data was delayed by several bytes being sent/received for an echo-test program I wrote. It seems like the SPI component has an internal FIFO buffer for both input and output, which could be why you are having a delay between seeing the byte on the physical line, and seeing it in the RX buffer in the component. I ended up rewriting my communications protocol to be ignorant of timing by introducing start/end of data sequences that allow me to merely send a data message and ignore all data until a response comes in. This allowed a more or less polling of the data until the next message start sequence.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I ran into a similar issue when setting up the SPI component to communicate with a Microchip SPI device; I ran into the issue where the data was delayed by several bytes being sent/received for an echo-test program I wrote. It seems like the SPI component has an internal FIFO buffer for both input and output, which could be why you are having a delay between seeing the byte on the physical line, and seeing it in the RX buffer in the component. I ended up rewriting my communications protocol to be ignorant of timing by introducing start/end of data sequences that allow me to merely send a data message and ignore all data until a response comes in. This allowed a more or less polling of the data until the next message start sequence.