Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

 What can we do to test linearity (INL) of 12bit SAR ADC with sinusoidal signal source which has only 10bit DAC ?

   

Simply put how can i increase linearity performance of 10bit DAC source?

   

Appriciate your comments

   

Thanks

0 Likes
16 Replies
Anonymous
Not applicable
        Will PWM and LPF use for it?   
0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Is there a reason you are restricted to a 10 bit DAC? Why not using one with a higher resolution (even using 12-bit one will give you the problem that the DAC itself might not be linear).

   

And what is the reason for you to test the linearity of the ADC at all?

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

You might want to read Jim Williams on such a matter: cds.linear.com/docs/en/design-note/dsol11.pdf

   

Also, you can use two IDACs, one with low current and the other one with high current, and combine their outputs. There is a white paper available: www.cypress.com/

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Use dithered dac component as one possibility -

   

 

   

http://www.cypress.com/?rID=86073

   

 

   

http://www.cypress.com/?rID=47478

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Thank you @hli 

   

Its more of query whether it is possible to improve linearity of DAC by any simple means.

   

If we wanted to use 10bit source and improve its SNR  then we could just use a bandpass filter followed by buffer ryt ?

   

In a similar way is there anything we could do to improve linearity of source, if yes please explain briefly.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given
0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Yopur original question was about resolution, not about linearity of the DAC. So now I'm confused...

   

If you want to improve the resolution, look at the documents Dana I gave you. They show multiple ways to increase the resolution of the PSoC IDACs up to 12 bit. If you need better resolution, you can a PWM as DAC as PSoC73 suggested.

   

If you want to improve the DACs linearity, ask Dana, she knows her stuff 🙂 (Much better than I do, I should add...)

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

It might be useful if you could shed some light on -

   

 

   

1) Target specs needed, DC, AC, temp, noise......

   

2) Application, what is the DAC output being used for

   

 

   

A filter and buffer can improve noise performance, or destroy it, it all

   

depends on specs you are trying to achieve and how you implement

   

the additional signal path components. As you approach higher perfformance

   

very subtle effects cause increasing problems, like the crossover distortion

   

in the input of R-R OpAmps the industry does not like to talk about.....

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 thank you.

   

@hli my question was how can i improve the linearity of 10 bit DAC such that it is equivalent to a 12bit DAC source.

   

@dana application my source is limited and i would like add some external circuitry to improve its linearity so that i can test ADC with that. So the question is what external circuitary should i add to serve this purpose ?

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Your first question, dithering, per link posted in prior part of thread.

   

 

   

One approach to SAR testing, use 16 bit PWM with integrator ( R-C network ), DelSig to read PWM

   

output of R-C, and feed R-C to SAR. Since DelSig good to 20 bits, that in turn insures you know what

   

the V source (PWM) is doing, and measure against SAR output. I would use averaging on readings to eliminate

   

un-correlated noise.

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Scratch the SAR testing comment in prior post, forgot there is no DelSig

   

in PSOC 4.

   

 

   

If you used 16 bit PWM approach, and supplied a precision reference for Vdd on the

   

part, then PWM would in effect become a precision DAC. Note this is only if you need

   

absolute accuracy. If all you need is relative no reference is necessary. The PWM is

   

inherently montonic, only its output integrator, if you used an OpAmp integrator vs the

   

simple R-C network, would affect montonicity.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Thank you dana

   

can you provide any sample project file in which PWM is used a DAC.

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Did you look at the first two links Dana gave you? The contain an AppNote about increasing the resolution of the PSoC DACs, and even a complete dithered VDAC (which I didn't knew existed as finished component - thanks for pointing me to it, Dana!)

0 Likes
lock attach
Attachments are accessible only for community members.
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Place a PWM, and then you control its duty cycle which when integrated

   

yields a DC outoput directly proportional to DC.

   

 

   

Attached some ref material for computing filter components.

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

"yields a DC outoput directly proportional to DC."

   

 

   

That might be confusing in prior post, should be

   

 

   

"yields a DC output directly proportional to Duty Cycle."

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

 Thank you dana.

0 Likes