Other Technologies Forum Discussions
Browse the Community
Featured Discussions
Hi,
I am looking for phase noise specifications for the CY22394 clock generator. Where can I find information on noise performance?
Thanks,
Jim
Show LessHow does a software interact with hardware? Can someone explain me. 🙂
Hi supporters,
I would like to confirm crystal specifications for CY25560SXI.
ESR ,Drive level ,frequency tolerance ,and so on.
I can not find recommended crystal specifications on the datasheet.
Regards
Junichi Nagata
Show Less
Hello
We got the TPMS test instrument (GWINSTEK C1100) as a transmitter to send TPMS data and the TDA5240 tester board as a receiver.
The left side of the attached photo is the instrument set to send out the TPMS data (preamble: N/A, SYNC: 0, DATA: F94A2BF94A2BF94A2BF94A, Coding: Manchester, Baudrate:19200), and right side of the attached photo is TDA5240 B12 explorer to receive the data.
You can see the TDA5240 explorer shows that “payload comparison not OK” on Received packets and there is no correct received payload at all.
Please help check is there any setup is wrong for TDA5240 or the instrument, thanks a lot.
Show LessIn general power switching circuits, the purpose of controlling power is to save power and control quiescent current. However, the following circuit has several disadvantages:
1. The pressure drop of the tube is large
We know that the saturation voltage drop of the PNP tube as the switch tube is 0-0.3V, which is unacceptable in low-voltage circuits. The maximum error of the 3.3V control power supply becomes 3V, and some 1.5V power supply becomes 1.2V, which will cause damage to the chip powered by it.
The tube pressure drop of PMOS is Vdrop=Id×Rdson, Rdson can be selected, and the actual value is within 1 ohm.
2. Control current
We know that Ib and Ic are related, and the saturation amplification factor is generally designed to be 30, so when we pass a current of 200mA, Ib=200/30=7mA, which leads to a large power consumption of the control circuit.
3. Switch tube power consumption
We know that the power consumption calculation formula of the triode is Pd=Veb×Ib+Vec×Ic. When Vec is saturated, under the condition of 0-0.3V, when the passing current is large, the power consumption of the switch tube will be very large.
In comparison, the on-resistance Rdson of PMOS is small (also optional), P=Rdson×Id^2.
PMOS high voltage circuit design (12V) circuit
Comparing PNP circuit design
Low voltage switch (NMOS) [5V, 3.3V, 1.5V]
NMOS turn-off conditions:
Here, the PNP tube is used to directly conduct the G and Vin of the NMOS, so that the NMOS can be completely turned on. If Vin cannot be completely connected to the G of the NMOS, use the top PMOS solution. If the connection is as follows :
Result:
When Photo Control is set to high level, 9014 is turned on and 640 is turned off. When Photo Control is at low level, 9014 is disconnected and 640 is turned on, but at this time, the voltage drop between ds on 640 is 3~4V, the original intention is DC=VBAT(8V), and now the DC is only 3 volts;
Reason:
Only NPN+PMOS is used for power control, this is NPN+NMOS, R21 can be directly replaced with 0 ohms, but nothing is controlled.
In addition, the substrate of NMOS is generally connected to the source when it is made. The NMOS needs to control the voltage (relative to the substrate) to be greater than the turn-on voltage when it is turned on. In this way, the substrate is completely suspended. No matter how the current circuit is controlled, it can reach If the requirements are not met, the design of the circuit itself is wrong. NMOS is generally used for low output, and PMOS is for high output circuit. This property is similar to that of NPN and PNP of triode. Transistors are used in TTL, TTL can drive MOS, and MOS cannot drive TTL.
Editor: Perceptive-IC
Show LessPer the photo of the cable #GATELEAD500PB346, is it defective? Please advise
While using the program provided - ClockWizard 2.1 to configure the CY27410, it was noted that the register addresses, e.g. 0x000000, 0x0186A0, are 24 bits long listed in the memory map of the results tab. This seems to contradict the information on I2C communication found in the datasheet.
On page 8 of 30 in Document Number: 001-89074 Rev. *M, it is documented that "A valid write operation must have a full 8-bit register." Furthermore, on page 9 of 30 on the same document, the following is noted: "... the CY27410 issues an acknowledge and transmits the 8-bit word."
It is clear that the datasheet of the CY27410 states that it reads and writes 8-bit words.
My question is then, why does the program ClockWizard 2.1 suggest that the addresses are 24 bits long, identified by the hex addresses listed in the results tab in the memory map section.
Show LessHi ~
We got the TPMS test instrument (GWINSTEK C1100) as transmitter to send TPMS data and TDA5240 tester board as receiver.
The left side of attached photo is instrument setting and to send out the TPMS data (preamble: N/A, SYNC: 0, DATA: F94A2BF94A2BF94A2BF94A, Coding:Manchester, Baudrate:19200), and right side of attached photo is TDA5240 B12 explorer to receive the data.
You can see the TDA5240 explorer show that “payload comparison not OK” on Received packets and there is no correct received payload at all.
Please help check is there any setup is wrong for TDA5240 or instrument, thanks.
Show Less