Other Technologies Forum Discussions
Browse the Community
Featured Discussions
Hello,
some sellers propose CY22801KSXC-024 ICs,
when I wrote this post and filled the field 'Associated Product', CY22801SXC-038 was automatically proposed as one of selectable product in the list.
What -024 and -038 mean?
In datasheet these parameters mean 'Custom Configuration Code (Only for Factory Programmable Devices)'.
Is it possible to find the frequencies for these ICs?
For example,
under Fref = ??? MHz
CLKA = ... MHz, CLKB = , CLKC= .
Show Less
Hello
Does Infineon have any solution for IEC-1000-4-6 (not IEC 1000-4-5)) who applies RF (150K~8M)stress
which is current injection ?
Customer says TVS is not valid for this ( current- type noise), and customer's product is small for using Big-size
choke coil...
Please advise.
Thank you for your cooperation
Show Less
Good Afternoon,
I am looking for a BSDL file for CY37512VP208-66NC / 5962-9952601QZC (208 QFP). I would like to run a JTAG IDCODE test on these components, in order to do so I have been looking for the BSDL file but can not seem to find it .
-Thank You
Show LessKTY23-5 or KTY 23-5 is Active or obsolete
Hi Teams,
I want to check the Drawing of Tape and Reel information.
The target parts are MB3771PF of CYPRESS.
This part has been discontinued and no information can be found.
Thanks and Best Regards,
Show Less
Hello, I have question about Legacy-Cypress CY7B923JXC, CY7B933JXC Devices
https://www.cypress.com/file/136191/download
I can find "Consumption current at Freq=MAX, transmitter side ICCT=65mA(typ), 85mA(max),
Receiving side ICCR = 120mA (typ), 155mA (max) consumption current" is specified.
Please let me know current consumption when Freq is more low (specifically 167.77Mbps).
thanks
Show LessInfineon担当者様
御社で買収したCYPRESSのMB3771PF-G-BND-JN-ERE1 のTape and Reelの形状について確認したいのですが図面はないでしょうか?
DatasheetにはPackgae形状はあるのですがTape and Reel形状はありませんでした。
外注先の搭載業者から問い合わせがあり仕様を探しているところです。
お手数をおかけしますがご確認お願い致します。
Show Less