Browse the Community
Recent discussions
Why might the output be inverted?
A board using CY2308SXI-1 seems to be inverting the output on bypass mode (S2=1; S1 =0).
But according to the data sheet the output is only inverted from the reference clock for the -2 or -3 devices.
Note: R57 not installed
G
Show LessGood day !
This is Ken Nam from Hwasung G&I located in republic of Korea.
We are manufacturer & supplier for OTIS Elevator dealing with PCB, Control Panel, Cable Harness.
We have been supplied Cypress Cy7c53150-20AXI for PCB Application so far, but as you know the cost and stock issue kept occurred..
So it makes us difficult sourcing it lately.
For solution we look for any replaceable or the most similar type that can work on our PCB.
Could you help us with it and let us know part# that can replaceable for Cypress Cy7c53150-20AXI?
Thank you
NAM
Show LessHello,
the BCW66K has a thermal resistance of 70K/W @TS=115°C compared to 215 K/W of the BCW66. Is there really a difference in the thermal design or is it just a different presentation methode? I know that the BCW66 is obsolet, but I want to understand the difference in the two datasheets.
Regards
M.M.
BCW66K
BCW66
Show Less
Hi,
I would like to buy the "SP4XDEVKITTOBO1" development board (https://www.infineon.com/cms/en/product/evaluation-boards/sp4x_dev_kit/#) but unable to find any order information and already check on eTailers site for this evolution board.
I really appreciated if someone could please guide me into correct direction ASAP to place an order for this.
Thanks,
-Abhi
Show LessI'd like use the TCA 355 for proximity switch product. Could you please provide manual regarding how to calculate inductive distance of components TCA355? and how to steady the inductive distance caused by ambient temperature variation? any compensation design proposal?
Show LessI just came into contact with Labview, designed a product counter, and asked how to wire the photoelectric sensor and the capture card. After I connected it, it was an NPN type, that is, it outputs a low level when an object is blocked, and the program I designed is a low power When the pin goes high, the count is +1, and now when I click to run the program, it will change the count from 0 to 1 without doing anything. Is there a PNP connection between the sensor and the acquisition card?
Show LessBuenos días,
He comprobado que el sensor DPS 310, no mide bien la temperatura; si partimos de 25º como como base, a 0º aporta datos en el entorno de -2.5º ó -3º. El error es progresivo. Lo he comparado con otros sensores como TMP-117, BMP388, DC-1080 y otros, los datos difieren de todos ellos.
He utilizado diferentes librerías de ARDUINO, siempre con los mismos resultados.
¿Alguien puede ayudarme a resolver el problema?.
Gracias y un saludo.
Show LessHi there, is it possible to use INA3221 Current Sensor to measure only voltages at the three output channels without anything on the input bus? I am wondering if it is possible to use this module in a reverse direction, and have CH1, CH2 and CH3 voltage readings separately and maybe then allow CH1 to pass through the input bus using a switch transistor. Something like a voltage detect and then passthrough in the opposite direction from CH1 CH2 CH3 to input bus.
Show LessI used the accelerometer sensor of the PCB, and cooperated with the NI 4461 acquisition card to perform a vibration signal of an insect, and obtained such a signal. It stands to reason that the sensitivity of this sensor is very high. But even if I tap the tabletop that touches the sensor with my hand. The change in this waveform on the graph is also not obvious. Where is the problem? PS: Because my computer does not have a PCI slot, I bought a CPI-E to CPI interface, and then used an extension cable to connect the capture card to the computer. Does it matter?
CY37256P160-100AI --- can you please let us know the EOL date for this part