Other Technologies Forum Discussions
Browse the Community
Featured Discussions
Does anyone know the production status of the PN IRFY044CM? It's a MOSFET N-Channel. It's not on the Infineon website. However, I found a datasheet for the part. https://www.irf.com/product-info/datasheets/data/irfy044c.pdf. Thank you for your help.
Show LessHave an IC (TSOP6) with the type code AGs (and the number 35).
The "s" may indicate that it is a Siemens and now Infineon circuit.
Does anyone know what this circuit may be?
Show Less
Hello
Do you have Maximum downward pressure Spec of CY7B923JXC, CY7B933JXC(PLCC28) for heat sink.
We are a group of students from the Wirtschaftsakademie Nordakademie in the north of Hamburg.
As part of a project for the module Innovation Management, we are looking for alternative application areas for a platform-based surface analysis tool.
In the course of this, we are using the ISAA method to find alternative areas of application by explaining the advantages of the technology.
Does anyone know of a problem area/area of application where the following benefits could be advantageous (there is no industry fixation here, the more creative the better)?
The platform offers:
(Soil) surface analysis based on satellite images
Bundling and processing of operational data in the forum
Integration of weather data (forecast and history)
Live communication (colleagues, employees, etc.)
Creation of biomass maps based on given and measured data
Many, many thanks in advance for your input!
I learn linker script recently and there are two commands which confused me. They are EXTERN and PROVIDE. In these article, it said EXTERN is force symbol to be entered in the output file as an undefined symbol. I try to add EXTERN(test) in the linker script and why can it compile and link successfully? I mean the test is undefined symbol, why can it link without any error? And for PROVIDE command, in my understanding, it is mainly avoid multiple definition and I try to add symbol test = .(without PROVIDE)in data section of linker script and declare variable int test in my source code, but why there is no error when linking? Shouldn't it be multiple definition error?
Show LessFirst off if this is not aloud, I'm sorry and please delete.
I'm a free lance AutoCAD operator. I came across a set of electrical drawings with Infineon name on them. I am always looking for ways to make my drawings more crisp and clear. Below is a snipit of the drawing I'm talking about. If there is someone that would be willing to help me figure out what font they use and how they get their drawings to look so crisp, it would be much appreciated.
Show Less
I am working on TDA5235 and I read the value of the serial numberr register (SN0 ~ SN3 register) to check the SPI.
When I checked, the serial number value didn't come out consistently.
So, I want to compare it to what is in the datasheet, but I don't know what that means.
What does "SN0.6 set to 1 and SN0.5 set to 0" mean?
Show Less
I'm looking for a smart card or any secure chip that supports version 3.1.0 of Java Card. According to my research, NXP JCOP 7 has this feature.
Is there exist the same product? Otherwise, Can you help me, how and where can I prepare it?
Infineon offers ESD and Surge protection @ https://www.infineon.com/cms/en/product/esd-and-surge-protection/
Are any of Infineon's protection components recommended for Lightning induced surge?
Greg
Show Less