Other Technologies Forum Discussions
Browse the Community
Featured Discussions
This SBC feature requires:
1. Converts 12V power to 5V 2. Has power
monitoring 3. Has a hardware watchdog 4. Supports CAN and CANFD communication 5. Supports wake-up
6. Comes with functional safety ASILD and safety manuals and other documents
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E5%85%B6%E4%BB%96%E9%80%9A%E7%94%A8%E6%8A%80%E6%9C%AF/%E5%B8%A6%E5%8A%9F%E8%83%BD%E5%AE%89%E5%85%A8ASILD%E7%9A%84SBC%E5%9E%8B%E5%8F%B7%E6%8E%A8%E8%8D%90/td-p/653425
Show LessHi Team
Kindly help to clarify on the Datecode which markings on the component.
I'm not sure which year the chip as below chart was produced.
Show Less
We use 'IR PowIRCenter' software. It was requested by SW to update, we start the process and it's stopped (the program was frozen). We restart the SW, but the device is not working and we can't restart the update procedure (error message - 'USBxxx_PowlRCenter.hex is missing').
And in the bottom of the window in the FW cell we see note – “bootloader” initially it was FW version here.
How we can repaire this programmer?
Where we can found FW for Silabs C8051F342 MCU? Show Less
Hi,
I would like to have confirmation whether the temperature sensor KT100 is really a non-RoHS compliant component.
At some distributors, it is marked as non-compliant but in the datasheet is no clear indication of that.
Can you please confirm the RoHS compliance status?
Thanks
Show LessWe are facing an issue wrt the installation of System Programmer in our PCs. Attached is the error message we are getting wherein it states to contact Infineon for the error. We have installed labview 2012 as per the software requirement prior to installation.
Kindly help us in rectifying the error.
Show LessI don't think there is a list of all the functions of the HAL library in the ROM and how to use it, which is necessary for creating firmware, in the published materials, but can I get it?
Or is it already published somewhere?
Please let me know. Thank you.
Show LessHello
My customer is looking for TVS with Low clamping voltage ( below 10Volts) at IEC61000-4-2 for Vrwm=5V.
The competitor is uClamp0501T. ( I attached the capture of data sheet for comparison)
Yes, Customer knows competitors product -test condition is 2.5Gs/s, and also ours are 20Gs/s, ( so high) but
he says Vcl= 5.6V is so low....
<Criteria>
*Vrwm=5V
*Either Uni-direction/Bi-direction OK , Either 1-protected line/2-protected line is OK . ( 1-line is better)
*Vcl should be lower ( lower than 10V, hopefully.)
<Question>
Would you advice me the part number for replace the competitors part uClamp0501T ?
I think ESD230-B1-W0201 is the best solution for replace, also, ESD5V3U2U may be OK.
Best Regards
Show Less
Is there a simulation model such as the Spice model for ESD231B1W0201?
ESD231-B1-W0201 - Infineon Technologies
Show LessHello,
some sellers propose CY22801KSXC-024 ICs,
when I wrote this post and filled the field 'Associated Product', CY22801SXC-038 was automatically proposed as one of selectable product in the list.
What -024 and -038 mean?
In datasheet these parameters mean 'Custom Configuration Code (Only for Factory Programmable Devices)'.
Is it possible to find the frequencies for these ICs?
For example,
under Fref = ??? MHz
CLKA = ... MHz, CLKB = , CLKC= .
Show Less