Other Technologies Forum Discussions
Browse the Community
Featured Discussions
Hello everyone,
I recently came across news suggesting that the upcoming iPhone 15 will replace the Lightning port with USB-C. What are your thoughts on this potential change? Do you see it as a positive move, or are there concerns and considerations to discuss? Share your opinions and insights!
Thank you,
EHallPass
Show LessHi,
I'm looking for an Intel Microprocessor 8-bit bus interface converter/bridge to SPI that I'll implement at the FPGA in order to convert the FALC56 bus to another system SPI communication.
Does the intel Micropcoessor 8-bit bus interface have other names?
Show LessHey, We are building modular car with steer by wire technology in it. Upon calculations, we figure out the Torque and Power values for motors in Steering wheel and Steering Actuator, that is 11Nm and 240W respectively for Steering Actuator and 6Nm and 102W respectively for Steering Wheel. With turn radius 7 m and Wheel base being 2150 mm and Track width being 1280 mm, the inner and outer steering angle being 16.69 and 18.28 degrees respectively. It is also low top speed around 60-80 kmph. So, I need consultancy from Infineon on specifications provided and help us with acuring outsourced components. Thank you in advance.
Show Lesshello i would like to ask if infineon has an apparatus for entangled spintronic qubits. thanks very much.
There is not a lot of information on this topic. Show Less
Dear supporter,
I would like to translate the following KBA. Could you confirm?
Changed definition for the specification of tBIT(Bus) and tBIT(RxD) in TLE9371VSJ (infineon.com)
Best regards,
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/Community-Translation-Changed-definition-for-the-specification-of-tBIT-Bus-and/td-p/651593
Show LessHere am with TLE9471 board and am trying to communicate with it over SPI , as the initial SPI transaction testing am trying to read the contents of "Family and Product information Register" (0x7E00) over the SPI here am seeing received contents are "0x0000",
I believe as per the data sheet it should be 0x5F.
FYI, all the SPI configurations are matching to the SBC requirements and I have tried to send both upper & lower 16bits at a time and as well individually 8 bits, both cases am seeing same response.
Please do the needful in resolving it.
Thank you in advance. Show Less
Does anyone know the production status of the PN IRFY044CM? It's a MOSFET N-Channel. It's not on the Infineon website. However, I found a datasheet for the part. https://www.irf.com/product-info/datasheets/data/irfy044c.pdf. Thank you for your help.
Show Lesscould you please answer the following question we received via social media?
Question: Car (Petrol car?) becomes a smart car (EV?). How?
Here is the link to our post: https://www.facebook.com/345383962211058/posts/6028291123920285/?comment_id=236313525585188
Show Lesscould you please answer the following question we received via social media?
Question: I wonder, does the presentation cover the likely need to rip out one's existing central heating plumbing?
Link to the post: https://www.facebook.com/620993263398649/posts/651569123674396
Thank you
Show Less