Other Technologies Forum Discussions
Browse the Community
Featured Discussions
If not, what is the drop in replacement?
Hello,
Is the following product automotive compatible?
CY8CMBR3102
If not, can you offer us an equivalent automotive compatible product? (equivalent to the above product)
Thanks
Best Regards
Show LessAs a follow on to this closed discussion: https://community.cypress.com/message/187923
We’ve tried put ferrite beads, but it made the ripples worse, the aurora eye still close. We’ve built a brand new PWB board with CY2304SXI-2, so there is no need to rework, but the aurora eye still close. We are just wondering that why CY2304SXI-2 doesn’t perform like CY7B991V-5JXI, it is because CY2304SXI-2 has more jitter? It that possible you guys can send a technician to our lab for debugging?
This table is the test result for the old PWB board (it needs to rework in order to drop CY2304SXI into CY7B991V-5JXI footprint)
Aurora Eye | Other functions | Input support | |
CY7B991V-5JX | Open | Work | LVTTL |
CY2304SXI-2 | Close | Work | TTL |
CY2304SXI-1 | Close | Work | TTL |
Hi,
I am using the chips of Cypress recently. In out prevenient design, we were using the Clock Distribution Buffer chip, which is CY29940AXI.
But today I found that this chip is in the state of NRND, which means it can not be used anymore.
So, would you tell me that is there an alternative product of CY29940AXI?
And what is the new product's name?
Thank you so much and looking forward to your reply~~~
Show LessHave Cypress clock & buffer product roadmap for PCIe 4.0 application?
Thanks,
Mitchell
We have both parts in front of us and we do not get the CY27EE16ZEC-300 working.
I am looking for something similar to IDT MPC9855 to drive an NXP PowerQUICC III.
We find Cypress Clock Generaotor.Input differential signal (161.13Mhz),Output single-end signal (25Mhz),
Please help provide Cypress products (Part number) for package SOP8/SOP16 ?
Because instead of ICS840271I ,please refer to the attached file.
Requirement:
1.Input Frequency: 161.13MHz(differential)
2.Ouput Frequency: 25 MHz (Single)
3.Package : SOP8 / SOP16
Ex: Cypress CY27410 , but package SOP 48 Pin
Show Less