Other Technologies Forum Discussions
Browse the Community
Featured Discussions
How do I get Serial Port Viewer and Terminal to work on Parallels(Windows 10 on Mid 2012 MacBook Pro)?
Using part number CY7B992-7JI in an application with datasheet environment variables of F=80, C=50 and N=8, occasionally supply current values are observed in excess of the estimated 272mA max . As such, is 300mA a reasonable ceiling for supply current across a large sample of parts or is there another more aggressive limit that good parts would be sure not to exceed across the full temperature range for this device?
Show LessDear sir whether IC CY22150 can generate the variable pulse width clock or not?
有一個VCXO Phase Noise 測試問題, 當VC=1/2 VDD時, Phase Noise 測試會有spur產生
而如果避開VC=1/2VDD 就不會.
但是對於VCXO產品, 標準與客戶要求VC=1/2VDD 進行量測基本數據,那麼會有問題的?
請問Cypress 是否有建議的方案, 或後續是否有改善安排?
Show Less
Could somebody please advise functional or drop-in equivalents for Clock generator part CY22150 which is recommended for new design has a long life cycle expectation.
Show LessWe had measurement LVDS 1.8V 40Mhz~100Mhz RMS phase jitter performance about 1.0~1.5ps @12K-20M.
But datasheet only show fOUT = 156.25 MHz,12 kHz–20 MHz offset, non-VCXO mode MAX. is 250fs(0.25ps).
Could you help check 40Mhz~100Mhz bandwidth jitter performance 1.0~1.5ps @12K-20M are resonable?
Have any test data can share?
Thanks,
Mitchell
Show LessThis is for Commscope service/spare dept.
I am having a problem in production where the frequency output of the CY2291 is outside previously established tolerances. I am trying to calculate what the realistic tolerances should be following the discussion in https://www.cypress.com/file/42656/download. In order to do this, I need to know the process variation and voltage/temperature stability of the CY2291 (this is not listed in the datasheet). Can anybody provide these numbers?
Show LessIf not, what is the drop in replacement?
Hello,
Is the following product automotive compatible?
CY8CMBR3102
If not, can you offer us an equivalent automotive compatible product? (equivalent to the above product)
Thanks
Best Regards
Show Less