Other Technologies General Forum Discussions
Hi Community
Please tell me how to interface Hotlink Transmitter and Receiver with FPGA IC(Sparant 3E). I have attached the Hotlink Datasheet.
Show LessHello
We got the TPMS test instrument (GWINSTEK C1100) as a transmitter to send TPMS data and the TDA5240 tester board as a receiver.
The left side of the attached photo is the instrument set to send out the TPMS data (preamble: N/A, SYNC: 0, DATA: F94A2BF94A2BF94A2BF94A, Coding: Manchester, Baudrate:19200), and right side of the attached photo is TDA5240 B12 explorer to receive the data.
You can see the TDA5240 explorer shows that “payload comparison not OK” on Received packets and there is no correct received payload at all.
Please help check is there any setup is wrong for TDA5240 or the instrument, thanks a lot.
Show LessIn general power switching circuits, the purpose of controlling power is to save power and control quiescent current. However, the following circuit has several disadvantages:
1. The pressure drop of the tube is large
We know that the saturation voltage drop of the PNP tube as the switch tube is 0-0.3V, which is unacceptable in low-voltage circuits. The maximum error of the 3.3V control power supply becomes 3V, and some 1.5V power supply becomes 1.2V, which will cause damage to the chip powered by it.
The tube pressure drop of PMOS is Vdrop=Id×Rdson, Rdson can be selected, and the actual value is within 1 ohm.
2. Control current
We know that Ib and Ic are related, and the saturation amplification factor is generally designed to be 30, so when we pass a current of 200mA, Ib=200/30=7mA, which leads to a large power consumption of the control circuit.
3. Switch tube power consumption
We know that the power consumption calculation formula of the triode is Pd=Veb×Ib+Vec×Ic. When Vec is saturated, under the condition of 0-0.3V, when the passing current is large, the power consumption of the switch tube will be very large.
In comparison, the on-resistance Rdson of PMOS is small (also optional), P=Rdson×Id^2.
PMOS high voltage circuit design (12V) circuit
Comparing PNP circuit design
Low voltage switch (NMOS) [5V, 3.3V, 1.5V]
NMOS turn-off conditions:
Here, the PNP tube is used to directly conduct the G and Vin of the NMOS, so that the NMOS can be completely turned on. If Vin cannot be completely connected to the G of the NMOS, use the top PMOS solution. If the connection is as follows :
Result:
When Photo Control is set to high level, 9014 is turned on and 640 is turned off. When Photo Control is at low level, 9014 is disconnected and 640 is turned on, but at this time, the voltage drop between ds on 640 is 3~4V, the original intention is DC=VBAT(8V), and now the DC is only 3 volts;
Reason:
Only NPN+PMOS is used for power control, this is NPN+NMOS, R21 can be directly replaced with 0 ohms, but nothing is controlled.
In addition, the substrate of NMOS is generally connected to the source when it is made. The NMOS needs to control the voltage (relative to the substrate) to be greater than the turn-on voltage when it is turned on. In this way, the substrate is completely suspended. No matter how the current circuit is controlled, it can reach If the requirements are not met, the design of the circuit itself is wrong. NMOS is generally used for low output, and PMOS is for high output circuit. This property is similar to that of NPN and PNP of triode. Transistors are used in TTL, TTL can drive MOS, and MOS cannot drive TTL.
Editor: Perceptive-IC
Show LessRecently I got a batch of IR2156STRPBF with D/C of 12+...And the package name is D2-PAK, I have searched all the websites and have never seen IR2156STRPBF in this package form. Please check the picture. Can anyone tell whether it is real or fake? Many thanks in advance...It's really important to me.
Show LessHow to get UID on SLJ 52GDA128CC