Other Technologies General Forum Discussions
Hi all,
1)Please let me know the resistance value when ISO1I811T isn’t connected to LED at TYP2.
2)The datasheet says “The specified switching thresholds may change if the resistor is used.”
Could you please tell me what value in the datasheet is the specified switching thresholds?
Best regards,
MS
I cannot find any information about the above models on Infineon. com. Please inform me of the differences of the three models and whether any two models of them are substitutes for each other.
Show LessHi all,
Is there a sequence for rising/falling between VBB and VCC?
Best regards,
MS
Hi all,
The value of Digital Filter Monitoring Time when fscantyp is 100k is as follows.
Is it correct that this value is multiplied by 100k/125K when fscantyp is 125kHz?
Best regards,
MS
Dear Colleagues, in the datasheet, table 2 shows that the SCV function only can be detected in the inactive mode, and in active mode, if SCV really happened, OLA will be reported instead of SCV because SCV is not distinguishable from OLA.
based on the Diagnostics Overview
My understanding: in active mode, even SCV really happened, we do not have the function to detect this "unwanted" mode, but OLA can be detected if happened. SCV cannot be detected in active mode.
I am not sure if I understand this in the right way, please help confirm.
Thank you.
Show Less
Hello,
I would like to place the ESD106-B1-W0201 at the base of the transmit antenna (RF power: 23dBm). Do you have experience with this type of use?
Or will it work?
Are there any precautions when placing the ESD106-B1-W0201 at the base of the antenna?
Best regards,
Nakamura
How does a software interact with hardware? Can someone explain me. 🙂