Other Technologies General Forum Discussions
Sort by:
Other Technologies General
Hello,I would like to use NovalithIC™ BTN7970 High Current PN Half Bridge, at the switching frequency ~1 kHz. The trouble is that I need to modulate p...
Show More
Hello,
I would like to use NovalithIC™ BTN7970 High Current PN Half Bridge, at the switching frequency ~1 kHz. The trouble is that I need to modulate pin No. 3 (Inhibit) as well to disable reverse current through the lower switches (therefore it would be switched at ~2 kHz). Is this possible, can BTN7970 respond properly to such relatively fast switching of this pin, since it goes to "sleep mode"?
Thank you! Show Less
I would like to use NovalithIC™ BTN7970 High Current PN Half Bridge, at the switching frequency ~1 kHz. The trouble is that I need to modulate pin No. 3 (Inhibit) as well to disable reverse current through the lower switches (therefore it would be switched at ~2 kHz). Is this possible, can BTN7970 respond properly to such relatively fast switching of this pin, since it goes to "sleep mode"?
Thank you! Show Less
Other Technologies General
Hi,TUS9090 supports DVB-T and DVB-H. This tuner can provide 4 different bandwidths, which are 5,6,7,8MHz respectively. The tuner adopts a direct conve...
Show More
Hi,
TUS9090 supports DVB-T and DVB-H. This tuner can provide 4 different bandwidths, which are 5,6,7,8MHz respectively. The tuner adopts a direct conversion receiver structure. It includes a complex filter to eliminate out-band noises. Is this bandwidth of the complex filter configurable?
Thanks a lot! Show Less
TUS9090 supports DVB-T and DVB-H. This tuner can provide 4 different bandwidths, which are 5,6,7,8MHz respectively. The tuner adopts a direct conversion receiver structure. It includes a complex filter to eliminate out-band noises. Is this bandwidth of the complex filter configurable?
Thanks a lot! Show Less
- « Previous
- Next »