Other Technologies General Forum Discussions
could you please answer the following question we received via social media?
Question: Car (Petrol car?) becomes a smart car (EV?). How?
Here is the link to our post: https://www.facebook.com/345383962211058/posts/6028291123920285/?comment_id=236313525585188
Show Lesscould you please answer the following question we received via social media?
Question: I wonder, does the presentation cover the likely need to rip out one's existing central heating plumbing?
Link to the post: https://www.facebook.com/620993263398649/posts/651569123674396
Thank you
Show LessMy device address CY8C9520A-24 is set via the "extentable soft addressing" function to 0x23.
I observe that the device performs clock stretching not only when interrogated on its address, but also on the addresses of other devices with different addresses.
Is it normal?
I attach some waveforms.
In the first the clock stretching on the address 0x23 in the attempt to read the register 0x0A.
In the following the clock stretching performed on the addresses of other devices, one present and one not connected.
Show Less
Have an IC (TSOP6) with the type code AGs (and the number 35).
The "s" may indicate that it is a Siemens and now Infineon circuit.
Does anyone know what this circuit may be?
Show Less
Hello
Do you have Maximum downward pressure Spec of CY7B923JXC, CY7B933JXC(PLCC28) for heat sink.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/CY7B923JXC-CY7B933JXC-PLCC28-Maximum-downward-pressure-Spec-for-heat-sink/td-p/616432
Show Less
Hello
Does Infineon have any solution for IEC-1000-4-6 (not IEC 1000-4-5)) who applies RF (150K~8M)stress
which is current injection ?
Customer says TVS is not valid for this ( current- type noise), and customer's product is small for using Big-size
choke coil...
Please advise.
Thank you for your cooperation
Show Less
We are a group of students from the Wirtschaftsakademie Nordakademie in the north of Hamburg.
As part of a project for the module Innovation Management, we are looking for alternative application areas for a platform-based surface analysis tool.
In the course of this, we are using the ISAA method to find alternative areas of application by explaining the advantages of the technology.
Does anyone know of a problem area/area of application where the following benefits could be advantageous (there is no industry fixation here, the more creative the better)?
The platform offers:
(Soil) surface analysis based on satellite images
Bundling and processing of operational data in the forum
Integration of weather data (forecast and history)
Live communication (colleagues, employees, etc.)
Creation of biomass maps based on given and measured data
Many, many thanks in advance for your input!
Good Afternoon,
I am looking for a BSDL file for CY37512VP208-66NC / 5962-9952601QZC (208 QFP). I would like to run a JTAG IDCODE test on these components, in order to do so I have been looking for the BSDL file but can not seem to find it .
-Thank You
Show Less