Other Technologies General Forum Discussions
text.format{('custom.tabs.no.results')}
Dear supporter,
I would like to translate the following KBA. Could you confirm?
Changed definition for the specification of tBIT(Bus) and tBIT(RxD) in TLE9371VSJ (infineon.com)
Best regards,
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/Community-Translation-Changed-definition-for-the-specification-of-tBIT-Bus-and/td-p/651593
Show LessHere am with TLE9471 board and am trying to communicate with it over SPI , as the initial SPI transaction testing am trying to read the contents of "Family and Product information Register" (0x7E00) over the SPI here am seeing received contents are "0x0000",
I believe as per the data sheet it should be 0x5F.
FYI, all the SPI configurations are matching to the SBC requirements and I have tried to send both upper & lower 16bits at a time and as well individually 8 bits, both cases am seeing same response.
Please do the needful in resolving it.
Thank you in advance. Show Less
Hi,
I would like to have confirmation whether the temperature sensor KT100 is really a non-RoHS compliant component.
At some distributors, it is marked as non-compliant but in the datasheet is no clear indication of that.
Can you please confirm the RoHS compliance status?
Thanks
Show LessWe are facing an issue wrt the installation of System Programmer in our PCs. Attached is the error message we are getting wherein it states to contact Infineon for the error. We have installed labview 2012 as per the software requirement prior to installation.
Kindly help us in rectifying the error.
Show LessDoes anyone know the production status of the PN IRFY044CM? It's a MOSFET N-Channel. It's not on the Infineon website. However, I found a datasheet for the part. https://www.irf.com/product-info/datasheets/data/irfy044c.pdf. Thank you for your help.
Show LessI don't think there is a list of all the functions of the HAL library in the ROM and how to use it, which is necessary for creating firmware, in the published materials, but can I get it?
Or is it already published somewhere?
Please let me know. Thank you.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/NAC1080%E3%81%AE%E3%83%95%E3%82%A1%E3%83%BC%E3%83%A0%E3%82%A6%E3%82%A7%E3%82%A2%E3%83%A9%E3%82%A4%E3%83%96%E3%83%A9%E3%83%AA%E5%86%85%E5%AE%B9/td-p/638504
Show LessHello
My customer is looking for TVS with Low clamping voltage ( below 10Volts) at IEC61000-4-2 for Vrwm=5V.
The competitor is uClamp0501T. ( I attached the capture of data sheet for comparison)
Yes, Customer knows competitors product -test condition is 2.5Gs/s, and also ours are 20Gs/s, ( so high) but
he says Vcl= 5.6V is so low....
<Criteria>
*Vrwm=5V
*Either Uni-direction/Bi-direction OK , Either 1-protected line/2-protected line is OK . ( 1-line is better)
*Vcl should be lower ( lower than 10V, hopefully.)
<Question>
Would you advice me the part number for replace the competitors part uClamp0501T ?
I think ESD230-B1-W0201 is the best solution for replace, also, ESD5V3U2U may be OK.
Best Regards
Show Less
Is there a simulation model such as the Spice model for ESD231B1W0201?
ESD231-B1-W0201 - Infineon Technologies
Show Lesscould you please answer the following question we received via social media?
Question: Car (Petrol car?) becomes a smart car (EV?). How?
Here is the link to our post: https://www.facebook.com/345383962211058/posts/6028291123920285/?comment_id=236313525585188
Show Less