Other Technologies General Forum Discussions
Hi, I have ordered CY8C9520A for 20 bit IO Expander,
The problem is that I can't find anything in the datasheet for basic circuit setup and testing.
Please advise.
Thanks
Clement
Show Less
Hello everyone,
I recently came across news suggesting that the upcoming iPhone 15 will replace the Lightning port with USB-C. What are your thoughts on this potential change? Do you see it as a positive move, or are there concerns and considerations to discuss? Share your opinions and insights!
Thank you,
EHallPass
Show Lessgreetings
according to cy3600i datasheet, ISR Programming software release 2.2 is required to program FLASH370i CPLDs.
we could not find setup file anywhere on the internet.
is it possible for infineon to share ISR Programming software release 2.2 download link?
thank you in advance
#cy7c374i
Show LessThis is my first time posting.
Please note that participation itself may be inappropriate for beginners in electronic circuits.
I am interested in the CY8CMBR series.
It seems that you can set up the device with an application called EZ-Click, but what kind of connection and operation do you need to use this application to set up the device you bought yourself instead of on the board?
I apologize for the inconvenience, but I would appreciate it if you could tell me.
Thank you in advance.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/%E8%87%AA%E5%88%86%E3%81%A7%E8%B3%BC%E5%85%A5%E3%81%97%E3%81%9FCY8CMBR3%E3%82%B7%E3%83%AA%E3%83%BC%E3%82%BA%E3%82%92EZ-click%E3%81%A7%E8%A8%AD%E5%AE%9A%E3%81%99%E3%82%8B%E6%96%B9%E6%B3%95%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E8%B3%AA%E5%95%8F%E3%81%A7%E3%81%99/td-p/658915
Show LessHi,
I'm looking for an Intel Microprocessor 8-bit bus interface converter/bridge to SPI that I'll implement at the FPGA in order to convert the FALC56 bus to another system SPI communication.
Does the intel Micropcoessor 8-bit bus interface have other names?
Show LessHi team,
Kindly assist us with below mentioned queries.
For the part series CY15B004Q-SXE* we need the following values:
1. Recommended operating temperature range
2. Thermal resistance of junction-board
looking for your soonest response.
Do I need to purchase the Infineon NFC Lock Mobile App Development Source Code Package to develop applications for NAC1080?
If you write code in each development environment according to the contents of smack-sdk-android-readme-1.2.0-4871.pdf 3 (for Android) and smack-sdk-ios-readme-1.3.1-6132.pdf 9 (for Iphone), you can use Source Is it possible to develop without Code Package?
Please let me know. Thank you in advance.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E4%BB%96%E3%81%AE%E3%83%86%E3%82%AF%E3%83%8E%E3%83%AD%E3%82%B8%E3%83%BC%E5%85%A8%E8%88%AC/NAC1080%E9%96%A2%E9%80%A3%E3%81%AE%E9%96%8B%E7%99%BA%E6%96%B9%E6%B3%95/td-p/650178
Show LessThis SBC feature requires:
1. Converts 12V power to 5V 2. Has power
monitoring 3. Has a hardware watchdog 4. Supports CAN and CANFD communication 5. Supports wake-up
6. Comes with functional safety ASILD and safety manuals and other documents
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E5%85%B6%E4%BB%96%E9%80%9A%E7%94%A8%E6%8A%80%E6%9C%AF/%E5%B8%A6%E5%8A%9F%E8%83%BD%E5%AE%89%E5%85%A8ASILD%E7%9A%84SBC%E5%9E%8B%E5%8F%B7%E6%8E%A8%E8%8D%90/td-p/653425
Show LessHi Team
Kindly help to clarify on the Datecode which markings on the component.
I'm not sure which year the chip as below chart was produced.
Show Less
Hey, We are building modular car with steer by wire technology in it. Upon calculations, we figure out the Torque and Power values for motors in Steering wheel and Steering Actuator, that is 11Nm and 240W respectively for Steering Actuator and 6Nm and 102W respectively for Steering Wheel. With turn radius 7 m and Wheel base being 2150 mm and Track width being 1280 mm, the inner and outer steering angle being 16.69 and 18.28 degrees respectively. It is also low top speed around 60-80 kmph. So, I need consultancy from Infineon on specifications provided and help us with acuring outsourced components. Thank you in advance.
Show Less