Other Technologies General Forum Discussions
Hello - I am looking for WarpISR Software for Device CY7C375i. Please help how to download.
In our project TC377TP micro is used. LIN1 is configured for LIN communication. Port pin 11.10 is Rx and 11.12 is Tx.
CANoe is showing invalid sync byte error.
What can be reason for the sync byte error. Show Less
Well, my friend has a volvo car, and his ECU is not working. His electrician said that the chip ,"Infineon 305 958 935" has burned and we cannot find another one, nor used one.
If you can send me some links of where I can buy this one it'll be great!
Thanks in advance!
Link of a photo of the chip: https://i.imgur.com/6wbTzA6.jpg
Show Less
I am trying to measure the motor current from the kits. The only thing I can find out is the 5m resistor is use to measure the current and connected to OP1 and OP2. Is there any code example to do this? I am new to micro-controller and trying to use this micro-controller for my project. Any suggestion is appreciated.
Thank you,
Eugene Show Less
I am new this group. I am currently looking for any support or documents related to Aurix TC397 MCAL multi core distribution in AUTOSAR architecture.
Kindly guide me . Show Less
我们在调试过程中发现STM32F427IIH6TR主机can perform 1-bit ECC correction and 2-bits ECC detection,
但是NAND Flash S34ML02G200BHI000 datasheet with 4-bit ECC per 528 bytes (×8) or 264 words (×16),从 Flash datasheet变更历史记录里面有提到ECC 从1bit变为4bit
请问以上有什么解决方案可以让NAND Flash和STM32之间ECC可以正常使用?谢谢!
Show Lessam presently working on DPS310 pressure sensor to enable interrupt on SDO pin,with QN9080 SOC
1.we want to read the data from fifo interrupt,how to read the fifo data
2.what are the registers to enable FIFO and read from FIFO
3. Plz share any sample reference,code or document or procedure for how to read the data from FIFO registers Show Less
Hello,
I'm making wireless switch USB with CYRF8935 module and MCU (ATmega48).
And I have some troubles with C coding.
I had read the datasheet several times, and set the registers according to the guide.
1)
Should I program the register in specific order?
I had just programmed register from 1 to 50 in order. I guess it's the biggest problem (maybe).
2)
CYRF8935 is programmed byte by byte, but some register(Reg52) has both read only and writable bit in one byte.
How should I program registers like this case?
3)
The packet structure is preamble + sync word + trailer + FIFO data. FIFO data are wrote in register 50, but I can't find the registers to program preamble and trailer.
Which registers are used to program preamble and trailer?
I'm beginner in transceiver and MCU, so I have too many troubles with programming. I attach the C code of Tx.
Thank you for reading. I really appreciate any help.
Thanks.
Show Less