Other Technologies General Forum Discussions
Show Less
Hello,
I plan to use the CY7C9689 TAXI compatible hotlink chip powered at 5V.
In the datasheet, the output level is VOH (min) = 2.4V. There is no typical values.
I plan to interface this component with a FPGA LVTTL compatible for a maximum 3.3V (+0.5V) input voltage.
Have you more recommendations for the TTL output voltage?
Show Less
During inspection, we observed that from the same date code there's:
1. Different die sizes
2. Different number of wires
3. Different country of diffusion. China n Philippines.
I cannot find any PCN on this on Infineon nor any public domain.
Can you advise if both are LOT are valid n share a copy of the PCN if it's available. Thank you! Show Less
Good morning,
I need to open a project based on a EEPLD CY7C374I.
Where may I find the WARP 3 version for a SUN machine? Unfortunately on the website it is not more possible to download this version.
Thank you very much
Show LessIs there any variation between Tasking Compiler used in Aurix Development Studio (ADS) and Actual Tasking Compiler?
Means Taking compiler with ADS has full capability or some features are disabled. Show Less
I am using Infineon ISO1H812G spi based output IC for my product development. According to datasheet and other referance links it has 1 Byte data buffer. when 1 byte value is write on the buffer
via SPI it operates the 8 outputs accordingly. After the system boot-up IC operates fine according to commands, but after some time it starts operating outputs randomly without writing any command.
It randomly starts ON/OFF the outputs after some time and did not respond to commands.
I have tried 2-3 ICs, but all the ICs are behaving same after some time.
I have used this IC for my another products, It works fine with them. I have observed this IC behaviour first time.
I wanted to know the reason behind this IC behaviour. Show Less
Hello, Working on a project with the CY7B933 in which the original design engineer has left. In the code that was left behind, was the reporting of status that included a received violation symbol, framing error, short frame and null counter. Typically these would be out of a chip, but it seems as if these are actually derived items in the application. My apologies for what should likely be found in the datasheet (is this the only document available) , but just looking for suggestions on where these parameters may be sourced.
Show Less当我使用CYP15G0101DXB这块芯片与FPGA进行数据交互时,发现CYP15G0101DXB发送给FPGA的RXCLK信号质量较差,因此FPGA无法利用该时钟信号对数据进行解析。
CYP15G0101DXB与FPGA并不在一块板卡上,带有FPGA的板卡通过接插件扣插在带有CYP15G0101DXB芯片的板卡上,发送与接收的传输速率设置为1250MBaud,但是将速率降低为800M或200MBaud时便能够收发正常。
请问当CYP15G0101DXB传输速率为1250Baud即RXCLK时钟为125MHz时,经过接插件信号质量就会变差吗?
Show Less
I have adapted the sample program "BLDC_HALL" from the Infineon download (IFX007T-Motor-Control-master) for my purposes.
I have currently connected a Maxon EC 45 flat with data sheet values:
- 3 Hall sensors
- 8 pole pairs
- Idle speed 6110 RPM
- No-load current 234 mA
- Nominal voltage 24V
Striking:
- the no-load current is 400mA
without the line after "void loop () {"
"PI_Update_Timeout = millis (); // updates the system time for better motor start"
the motor jerks and vibrates when it starts up in the "open loop"
I have the biggest problem with changing the speed.
Regardless of whether I change the "RefRPM" variable through serial input or by querying 2 digital pins (with button), nothing happens.
The BLDC motor always runs at the maximum possible speed
I would be very happy if someone could give me tips.
Many greetings
Klaus
Show Less
I am trying to test the sample code from Infineon on my TLE9862 Hardware. I have compiled the code using IAR compiler using the IAR startup file.
After flashing the code in the hardware my controller is getting reset continuously. Can someone provide me a working IAR startup file as I suspect this is an issue with startup file.
Thanks in advance. Show Less