Snap back voltage

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Not applicable
ESD3V3XU1BL & ESD3V3S1B have Vhold & Vtrig (snap back voltage)
How to know this information? Use TLP or add in IC datasheet
0 Likes
1 Reply
lock attach
Attachments are accessible only for community members.
AntonG
Employee
Employee
Hi Ken,

for ESD3V3XU1BL we specify following values:
Vtrig(min) = 5V
Vhold(min) = 4V
Vhold(typ) = 4.6V

Below you can find updated datasheet. I'm not sure why it's not available on product page, I'll look into it.


for ESD3V3S1B the values are the same as for ESD207-B1, which is a drop-in replacement product:
Vtrig(min) = Vhold(min) = 3.65V
Vhold(typ) = 4.4 V

Since ESD3V3S1B is discontinued, datasheet will not be updated. For new designs, ESD207-B1 is recommended:
0 Likes