F4-23MR12W1M1P_B11 short-circuit capability

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
User21259
Level 1
Level 1
First question asked First reply posted
Hi everyone,

I'm working on a 350V / 40A converter application and i intend to use the F4-23MR12W1M1P_B11 Infineon power module.

To protect my converter in a short-circuit case, i'm using a current sensor with 500 ns delay and i added a 6.6 uH inductor to slow the current rise, but i found that the inductor is taking too much place in the converter and there is no place left for other components, so i need to remove it. My question is :
In a short-circuit case, what maximal current i'm gonna get ? can the power module handle it ? if yes, for how much time ?

Thank you 🙂
0 Likes
0 Replies