Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

BASTIEN
Level 1
Level 1
First question asked Welcome!

Hello,

I plan to use the CY7C9689 TAXI compatible hotlink chip powered at 5V.

In the datasheet, the output level is VOH (min) = 2.4V. There is no typical values.

I plan to interface this component with a FPGA LVTTL compatible for a maximum 3.3V (+0.5V) input voltage.

Have you more recommendations for the TTL output voltage?

BASTIEN_0-1620107245404.png

 

1 Solution
Roy_Liu
Moderator
Moderator
Moderator
First comment on blog 1000 replies posted 500 solutions authored

Hi,

The VOH range is 2.4V - VDD(5.0V ±10%), the datasheet specifies the VOH as such, which means the pin is outputting high level as long as the VOH equal to or larger than 2.4V. In your case of interfacing a 3.3V FPAG to CY7C9689, you may consider using a voltage-level translator component between them.

Roy Liu

View solution in original post

0 Likes
1 Reply
Roy_Liu
Moderator
Moderator
Moderator
First comment on blog 1000 replies posted 500 solutions authored

Hi,

The VOH range is 2.4V - VDD(5.0V ±10%), the datasheet specifies the VOH as such, which means the pin is outputting high level as long as the VOH equal to or larger than 2.4V. In your case of interfacing a 3.3V FPAG to CY7C9689, you may consider using a voltage-level translator component between them.

Roy Liu
0 Likes