Not applicable
Jul 06, 2015
08:23 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Jul 06, 2015
08:23 PM
Building an LED Lamp with the RGB LED Shield is posted on the element14 Blog:
The Infineon RGB LED shield is spectacular for LED lighting. It is a complete, low-cost programmable board that can directly control up to three groups of LEDs with no additional components required.
The LEDs can be driven with a combined power of up to around 100W – perfect for home, commercial and industrial lighting applications.
This post investigates how to build an LED lamp with the RGB shield, LED module and heat sink.

Get all details in the e14 community:
http://bit.ly/element14_BuildAnLEDLamp
The Infineon RGB LED shield is spectacular for LED lighting. It is a complete, low-cost programmable board that can directly control up to three groups of LEDs with no additional components required.
The LEDs can be driven with a combined power of up to around 100W – perfect for home, commercial and industrial lighting applications.
This post investigates how to build an LED lamp with the RGB shield, LED module and heat sink.
Get all details in the e14 community:
http://bit.ly/element14_BuildAnLEDLamp
Labels
- Labels:
-
Technical Center
0 Replies