Recent discussions
Hi
I'm working on secure boot on TI omapl138 soc using TPM1.2 slb9645, I am able to detect TPM chip through I2C, But i didn't get any data sheet or technical reference module to know how TPM 1.2 works and register/memory addresses, To develop further can you please provide detailed documents of TPM 1.2 slb9645.
Thanks & regards
Yashwanth T L
Show LessHello All,
I'm trying to bringup TPM2.0-SLB9670VQ2.0 in "uboot2016" for IPQ8072 qualcomm chipset.
Would be great if some one pls share some docs/references or pointers.
thanks in advance..
Gourav Jain
Show LessHi Team,
Does Infineon have a TPM module which is FIPS 140-3 compliant or certified? I currently use SLB 9670VQ2.0 which is FIPS 140-2 certified and would like to move to FIPS 140-3.
Thanks and Regards,
Shahasan Noushad
Show Less
Hello, everyone, I bought an evaluation board iridium 9645 ( IRIDIUM9645TPMI2CTOBO1), with an SLB9645 TPM 1.2, but I can't find any datasheet to plug this board on a raspberry pi 3B (40 pins header). Could you provide the datasheet? If there is no datasheet, could you tell me what is the interest of the two jumpers, the 28 pins header, the 6 pins headers? The 26 pins header for raspberry? Where should I plug it on the header of my raspberry pi 3B, and in what way should I plug it?
Regards,
David
Show LessHi Infineon Team,
I'm trying to interface TI omapl138 soc with TPM1.2 slb9645 through Driver module (DM)_I2C, But facing problem with integration via U-boot not able to detect TPM chip on I2C bus. I'm looking for a U-boot driver/source code to interface TPM1.2 slb9645, Presently I am using U-Boot 2018.01.
Thanks & regards,
Yashwanth T L
Show LessWhat is the difference between VQFN-32-20 and VQFN-32-13? what 13 and 20 represents
Hi
Good day.
We have programming requirements for SLB9665 and SLB9670, and we are evaluating to implement TPM programming/provisioning to our programming systems. We have HSM and CA server, and we need the more detail information about LPC/SPI protocol and programming flow to implement. We have tried to find the source code from github, but it seems based on the OS to execute the IC provisioning.
May i know any documents about the detail (protocol and flow and command..) for third party?
Thank you.
Jack
Show Less
I am using HW with TPM module and with RHEL OS installed
We have binded password with Luks, so that we dont need to enter password on every boot.
when multiple abrupt power cycle happened, the TPM module got locked. I think DA lock happened.
1. How to come out from such lock out and recover automatically?
Regards
Jufail
Show Less
Is there any concern if OPTIGA TPM SLM9670 is located on a SPI bus, where other ICs such as SRAM and flash memory are connected to a CPU? SCLK, MOSI, and MISO signals will be driven even when CS# for TPM is negated. Is this OK?
Please kindly advise. Thanks,
Show Less