Hi @Sneha_P , I have found the problem that no link lib of abrmd. Thanks for your supporting.
Best reguards
Wen Zhu
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @wenzhu,
Please refer to this Application Note as a starting point to interface OPTIGA SLM9670 with RPi. If already interfaced, you can use these tools to test out the TPM functionalities: ELTT2 and Optiga TPM 2.0 Explorer.
For further public reference materials, please refer to our product page.
Hope this helps.
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
Hi @wenzhu,
There is no specific material for xczu19 of Xilinx Arm. Infineon TPM offeres reference application note of ARM platform which is RPi 3 or 4 under Linux environment to TPM2.0. You can bring up SLM9670 via SPI TPM2.0 driver under Linux, according to the setup of this.
Thanks,
Sneha
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P, thanks for your supporting, I have installed the /dev/tpm0 device and can see the information by eltt2 command. But how can I write private key to the SLM9670, I could not find some related references. Maybe you can give me more details information.
Best regards
Wen Zhu
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @wenzhu,
TPMs can generate private keys and store them securely. You can use TPM2_Create() and TPM2_CreatePrimary() to generate key pairs in TPM and usage of these commands are explained in the TCG Spec along with definitions of other TPM commands. This can be a starting point for understanding various commands and its usage.
Additionally, you can check TPM Explorer, which is a GUI-based tool for users to get familiarized with TPM2.0 quickly.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P, do you have Implementation examples of a Linux®-based Integrity Measurement Architecture using OPTIGATM TPM that I can refer?
Best regards
Wen Zhu
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
Hi @wenzhu,
TPM has a set of attestation features that can be used to perform authentication and protect the IMA measurement. More information on this can be found here: https://github.com/Infineon/remote-attestation-optiga-tpm
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
Hi @wenzhu,
As mentioned earlier, TPMs can generate private keys and store them securely. You can use TPM2_Create() and TPM2_CreatePrimary() commands along with owner authorization value to generate key pairs in TPM. Please refer to the TCG Command Spec for detailed explanation of these commands.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P , when execute command ' tpm2_createprimary', but take error. Can you give me some help? Print below:
tpm2_createprimary -c primary.ctx
** (process:1109): CRITICAL **: 00:02:08.409: failed to allocate dbus proxy object: Error calling StartServiceByName for com.intel.tss2.Tabrmd: Cannot do system-bus activation with no user
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:79:tcti_from_init() TCTI init for function 0xffff9cf04260 failed with a0008
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:109:tcti_from_info() Could not initialize TCTI named: tcti-abrmd
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:154:tcti_from_file() Could not initialize TCTI file: libtss2-tcti-tabrmd.so.0
WARNING:tcti:../tpm2-tss-3.0.3/src/util/io.c:252:socket_connect() Failed to connect to host 127.0.0.1, port 2321: errno 111: Connection refused
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tcti-swtpm.c:592:Tss2_Tcti_Swtpm_Init() Cannot connect to swtpm TPM socket
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:79:tcti_from_init() TCTI init for function 0xffff9c1679e0 failed with a000a
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:109:tcti_from_info() Could not initialize TCTI named: tcti-swtpm
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:154:tcti_from_file() Could not initialize TCTI file: libtss2-tcti-swtpm.so.0
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:254:tctildr_get_default() No standard TCTI could be loaded
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:416:Tss2_TctiLdr_Initialize_Ex() Failed to instantiate TCTI
ERROR: Could not load tcti, got: "(null)"
Best regards
Wen Zhu
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @wenzhu,
Could you try: ls -l /dev/tpm* to check if /dev/tpm0 or /dev/tpmrm0 exists. Also, if read/write commands work (tpm2_nv_write/read) from the tpm2-tools.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P , print below:
root@ORU3668_MAIN:~# tpm2_nvread
** (process:1140): CRITICAL **: 00:02:35.357: failed to allocate dbus proxy object: Error calling StartServiceByName for com.intel.tss2.Tabrmd: Cannot do system-bus activation with no user
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:79:tcti_from_init() TCTI init for function 0xffffa36f1260 failed with a0008
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:109:tcti_from_info() Could not initialize TCTI named: tcti-abrmd
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:154:tcti_from_file() Could not initialize TCTI file: libtss2-tcti-tabrmd.so.0
WARNING:tcti:../tpm2-tss-3.0.3/src/util/io.c:252:socket_connect() Failed to connect to host 127.0.0.1, port 2321: errno 111: Connection refused
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tcti-swtpm.c:592:Tss2_Tcti_Swtpm_Init() Cannot connect to swtpm TPM socket
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:79:tcti_from_init() TCTI init for function 0xffffa21449e0 failed with a000a
WARNING:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:109:tcti_from_info() Could not initialize TCTI named: tcti-swtpm
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:154:tcti_from_file() Could not initialize TCTI file: libtss2-tcti-swtpm.so.0
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr-dl.c:254:tctildr_get_default() No standard TCTI could be loaded
ERROR:tcti:../tpm2-tss-3.0.3/src/tss2-tcti/tctildr.c:416:Tss2_TctiLdr_Initialize_Ex() Failed to instantiate TCTI
ERROR: Could not load tcti, got: "(null)"
root@ORU3668_MAIN:~# Radio Service time out
root@ORU3668_MAIN:~#
root@ORU3668_MAIN:~# ls /dev/tpm*
/dev/tpm0 /dev/tpmrm0
root@ORU3668_MAIN:~#
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @wenzhu,
Can you try "sudo ldconfig" followed by "systemctl status tpm2-abrmd.service" and let me know the result of it?
To install tpm2-abrmd follow the steps provided in the INSTALL.md https://github.com/tpm2-software/tpm2-abrmd/blob/master/INSTALL.md
Note: These steps are for 2.0.0 of tpm2-abrmd and raspbian linux.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P , print below:
root@ORU3668_MAIN:~# service tpm2-abrmd status
Usage: tpm2-abrmd {start|stop|restart|force-reload|status}
root@ORU3668_MAIN:~# sudo ldconfig
root@ORU3668_MAIN:~#
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @Sneha_P , I have found the problem that no link lib of abrmd. Thanks for your supporting.
Best reguards
Wen Zhu