Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Anonymous
Not applicable

hello,

Im updating my design and need a replacmend for micron PC28F00AP30TFND (parallel nor).

i was thinking of S29GL01GT  however im having truble to find the appropriate CFI compatible with the old micron.

i dont know what to choose from this list:

Model Number (CFI Version, VIO, and VCC Range)
CFI Version 1.3
03 = V
IO = VCC = 2.7 to 3.6V, highest address sector protected
04 = V
IO = VCC = 2.7 to 3.6V, lowest address sector protected
V3 = V
IO = 1.65 to VCC, VCC = 2.7 to 3.6V, highest address sector protected
V4 = V
IO = 1.65 to VCC, VCC = 2.7 to 3.6V, lowest address sector protected
CFI Version 1.5
01 = V
IO = VCC = 2.7 to 3.6V, highest address sector protected
02 = V
IO = VCC = 2.7 to 3.6V, lowest address sector protected
V1 = V
IO = 1.65 to VCC, VCC = 2.7 to 3.6V, highest address sector protected
V2 = V
IO = 1.65 to VCC, VCC = 2.7 to 3.6V, lowest address sector protected

please help.

Thank you.

1 Solution

Hello,

If you do not use the RY/BY#, you can leave the pin open (floating).

Thanks,

Takahiro

View solution in original post

0 Likes
5 Replies
TakahiroK_16
Employee
Employee
100 replies posted 50 replies posted 25 solutions authored

Hello,

According to Micron's datasheet I found:

https://www.micron.com/~/media/documents/products/data-sheet/nor-flash/parallel/p30/p30-65nm_mlc_512...

The CFI version is 1.5.

pastedImage_1.png

I believe you are aware that the package pin-out and Vcc voltage range are incompatible between Micron PC28Fxxx and Cypress S29GL01GT and that's why you are 'updating' your design, correct?

Best Regards,

Takahiro

0 Likes
Anonymous
Not applicable

Hey,

thank you for your answer.

yes i know about voltage and pinout differences, couldnt find any compatibe part.

regarding the CFI V1.5- I didnt understand the differences between the options: highest /lowest address sector protected,

and the compatible mode in the micron.

in addition, does cypress has an example electrical schematics for the part?

please help.

thank you!

0 Likes

Hello,

If the WP# pin is Low, the highest (sector 1023) or lowest (sector 0) is protected from program/erase. This option select which one is protected. This function is not compatible with the Micron part. In the Micron part, all of sectors are protected if WP# is Low.

We don't have good example of schematics using this part.

Best Regards,

Takahiro

0 Likes
Anonymous
Not applicable

Hey,

in addition,is it possible to leave pin READY/BUSY (RY/BY#) open? (or it must be tied to GND?)

as i see, this pin is not needed during configuration of xilinx 7 series fpga (kintex).

thank you!

0 Likes

Hello,

If you do not use the RY/BY#, you can leave the pin open (floating).

Thanks,

Takahiro

0 Likes