s29al016j55tfnr10 equivalent part in AMD series

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
SAKA_3670866
Level 1
Level 1
First like given

Hi,

i'm using Nor Flash part no. s29al016j55tfnr10 in my design which  is 16 mega bit(1M x 16) top boot sector, which is programming using  the Codewarrior 8.8 Ide tool where the device is not listed in the existing devices.

The available devices are all of AMD series and s29GL series so i want to know the equivalent part in AMD series for my device, so that i can use same configurations for this one.

i also want to know what is the base address should be taken for this device, i'm using in word mode configuration(16 bit).

0 Likes
1 Solution

Hi Saiprakash,

Cypress' closest suggested migration path from the S29AL016J55TFNR10

is to the S29GL064S70TFB060 :

S29GL064S attributes :

     - 64-Mb  (no option for parallel NOR memory less than 64Mb)

     - 70nS access time only  (no option for 55nS)

     - available in 48-pin TSOP  (100% Pb-Free, RoHS Complaint) package

     - Auto., AEC-Q100 Grade 2, -40°C to +105°C  (no option for extend temp grade)

     - available in x16 (WORD mode), as Model 06 only

     - 64KB uniform sectors  (no option for 256KB sectors)

     - Does not have pin functions :  RY/BY# (pin-15);  BYTE# (pin-47)

     - Device ID :  x16 (WORD mode) Cycle-1 = 227Eh

                           x16 (WORD mode) Cycle-2 = 2213h

                           x16 (WORD mode) Cycle-3 = 2201h   

                         

URL to S29GL064S datasheet :

    https://www.cypress.com/file/177981/download  

All Am29LVxxx series have been discontinued under the AMD banner, and are not recommended for new designs.

Best regards,

Albert

Cypress Applications Support

    

View solution in original post

0 Likes
7 Replies
Apurva_S
Moderator
Moderator
Moderator
100 likes received 500 replies posted 250 solutions authored

Hi Saiprakash.

We are not aware about AMD series.

Kindly contact the customer support of AMD.

If you have any queries regarding Cypress parts, please let us know. We will be happy to help.

Best Regards,

Apurva 

0 Likes
SAKA_3670866
Level 1
Level 1
First like given

can you tell us the equivalent part of s29al016j55tfnr10 of this in cypress parts numbers only.

can you also please tell us what is the base address of this device,flash buff address and port size.

0 Likes

Hi Saiprakash,

AMD flash devices are obsoleted now. Since your IDE supports S29GL devices, you can go to the Cypress website (https://www.cypress.com/products/parallel-nor-flash-memory ) and take a look at the available GL devices. I would like to inform you that GL series will not have 16Mb parts.

The base address or the starting address of the device is 0x000000. It has A0-A19 address lines and DQ0-DQ15 data lines.

We are not clear about your question regarding flash buff address and port size.

Best Regards,

Apurva

0 Likes
SAKA_3670866
Level 1
Level 1
First like given

is this memory is protected or not protected after manufactured .If it is protected means how to un protect the memory .We had kept the WP pin to the LOW state.

0 Likes

Hi Saiprakash,

Could you please clarify which device are you talking about?

However I would like to inform you that for both S29AL016J and S29GL064S devices the WP# contains an internal pull-up; when unconnected, WP# is at VIH. And the device is shipped with all sector groups unprotected. When WP# is driven LOW it will protect the corresponding top or bottom sector.

Please let me know if you have any confusion.

Regards,

Apurva

0 Likes
SAKA_3670866
Level 1
Level 1
First like given

Any parallel nor flash device with 48 pin Tsop ---256k x 16 organization is still available with cypress ?

0 Likes

Hi Saiprakash,

Cypress' closest suggested migration path from the S29AL016J55TFNR10

is to the S29GL064S70TFB060 :

S29GL064S attributes :

     - 64-Mb  (no option for parallel NOR memory less than 64Mb)

     - 70nS access time only  (no option for 55nS)

     - available in 48-pin TSOP  (100% Pb-Free, RoHS Complaint) package

     - Auto., AEC-Q100 Grade 2, -40°C to +105°C  (no option for extend temp grade)

     - available in x16 (WORD mode), as Model 06 only

     - 64KB uniform sectors  (no option for 256KB sectors)

     - Does not have pin functions :  RY/BY# (pin-15);  BYTE# (pin-47)

     - Device ID :  x16 (WORD mode) Cycle-1 = 227Eh

                           x16 (WORD mode) Cycle-2 = 2213h

                           x16 (WORD mode) Cycle-3 = 2201h   

                         

URL to S29GL064S datasheet :

    https://www.cypress.com/file/177981/download  

All Am29LVxxx series have been discontinued under the AMD banner, and are not recommended for new designs.

Best regards,

Albert

Cypress Applications Support

    

0 Likes