Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

Currently evaluating this FLASH and attempting to lock registers using the WP# pin, however it's not working as advertised.

Using the WRR command I am able to set SRNV-1[SRWD]=1, which now should  follow WP#. I power cycle  and can verify

that  it is  set via UBOOT console using RDSR-1.

What I expect to happen is that if I ground WP# I should NOT be able to change SRNV1, however I am able to toggle this

register even with the pin grounded. What  am I missing? Thanks in advance.

0 Likes
1 Solution
Anonymous
Not applicable

Ok,

Believe we have found the issue, but still don't understand this fully. Our LINUX target boots up in single mode (MISO/MOSI), but when the kernel gets a hold of it, it runs in QUAD mode.

Somewhere  along the  way, it must have written to CRNV1 and set the QUAD_NV bit for QPI mode. This apparently has no effect on single mode operation, however it seems to prevent IO2 and IO3 to operate as WP# and RESET respectively. Once this was cleared, the write protection worked as expected.

View solution in original post

0 Likes
6 Replies