Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Nor Flash Forum Discussions

Sort by:
MAO
Nor Flash
The S29AL008J70BFI010 datasheet lists the sector trace time as "10s",The S29AL008J70BFI010 datasheet lists a maximum sector trace time of 10s.I unders... Show More
MAO
Nor Flash
S29PL032J70BFI120 and S29PL032J70BFI070What is the difference between these two products?Are there any differences between them?1) specification(2) us... Show More
ZELDAWIZARD
Nor Flash
Hi folks,  We use a S29GL01GT12DHVV10 for FPGA configuration memory. I am currently working on stress analysis and couldn't find any information in th... Show More
MAO
Nor Flash
PSCK/tCH/tCL are available as AC specifications for SCK duty ratio, and for tCH/tCL, Notes 30,Notes 30. ±10% duty cycle is supported for frequencies ≦... Show More
HiKu_1337496
Nor Flash
Hi, Please let me know processing across the boundary between Die1 and Die2 of S25HL02GT, For example, when program 32 bytes from 07FFFFF0h, is one tr... Show More
法尔额
Nor Flash

S29WS128P0PBFW000停产了,有替代的型号吗?

npatil15
Nor Flash
Hello Sir/Maam, I am using S29GL064S uniform sector flash memory in word mode, where I have successfully read the CIF Query data, but want to understa... Show More
igor_kuksiuk
Nor Flash
I have S25FL128S software blocked second half of address memory. Here is article describing this protection:  https://community.infineon.com/t5/Knowledge-Base-Articles/Block-Protection-Configuration-on-FL-S-and-FS-S-NOR-Flash-KBA224451/ta-p/253479... Show More
MustangCobra
Nor Flash
Regarding S25FL128SAGBHIA00, If I/O voltage is 3.3V, which is good for VIO/RFU ?1. "no connect".2. connect to 3.3V.   Best Regards, Hideki Show More
LIULIULIU123456
Nor Flash

S25FL256SAGMFIR01 这个型号丝印 FL256SAIFR0 是代表型号 第二行丝印 222QQ037 我想问这些数字还有字母分别代表什么含义 规格书上是没有显示的 能不能官方回复或者发一份正式说明文件给我

Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.