Nor Flash Forum Discussions
Parameter Sector Size of S25FL1-K is described N/A in data sheet.
On the other hands, that of S25FL-P is 4kB.
What is meaning of "N/A"?
Does "N/A" mean parameter sector is 1 byte?
Show LessDear Cyprocess developper community,
i would like to change an old memory flash for my design from S25FL164K0XMFI011 to S25FL064LABMFI011.
I find the attached document that explain the command change, but i don't know where to make that changement from my Psoc craetor project.
Sorry it may be easy for software engineer but i am an hardware engineer. Can you please help me ?
Thank you in advance for your support
Show LessHello,
We're working on a controller project targeted for S28HS256T / S28HS512T / S28HS01GT flash device.
When we set the flash model to OPI DDR, we noticed there's an extra DS pulse after every read.
Is this expected?
Attached is a screenshot of waveforms.
Thanks in advance.
Regards,
Lawrence
Show LessI am looking for the Junction-to-Board resistance, Junction-to-Case resistance, Max Junction Temperature, and Max Power Dissipated for S25FL064LABMFI010 SOIC8 package. I have only been able to locate the Junction-to-Ambient resistance in the data sheet. Thanks.
Show LessHi. cypress
In cypress internal system, I may find S35HL256 or S35HS256 is CRM active status as below and road map, but cypress offical website, I can't find the S35HL(HS)datasheet, whether we may introduce the S35 security PN to let customer to go to design in new project?or whether do you advise which type to promote?
Show Less
Hi ,
i have checked this parts & have a Obsolete document said the LTS in Oct-10-2009(DC 0941).
is it possible the parts still active in 2010? (DC 1022)
Thanks.
Show LessHi, Could you please help to provide the CY part number for replacing the below parts? Please advise the closest part number if no fully compatible option. MX25L12835FM2I-10G MX25L25635FMI-10G MX68GL1G0FUT2I-12G Thanks, Leon 12/16
Show LessI checked the data sheet and found that there was only thermal resistance of Theta JA (junction to ambient).
Can you tell me about the following two conditions?
- Thermal resistance of Theta JB (junction to Bord)
- Thermal resistance of Theta JC (junction to Case)
Target Device is S25FS512SAGMFI011.
Best Regards,
Kumada
Show LessWhere can I find MTBF data of 'S29JL064J70TF100' for reliability analysis