Nor Flash

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
bharris
Nor Flash
Hello,I am trying to write bit 3 of configuration register 3 in a S25HL250T device.  I see in the data sheet that the bit is only writeable in the non... Show More
peakjohn
Nor Flash
Is there any equal 4KB erase sector SPI Nor Flash solution in Infineon portfolios? I checked  in Semper series and S25FL/FS, S70FL/FS,  all of them ar... Show More
alikapatibabu
Nor Flash
Hi All,  We are using OSPI NOR Flash S28HS512TGABHM013 in our product. It would be great if you can share compatible driver for Linux-5.10.35 version.... Show More
adaml
Nor Flash
Hello everybody!   Recently I was doing some hacky/fancy tests of flash chip behavior between different manufacturers when it is used not *exactly* ho... Show More
devallap1
Nor Flash
Hi, I would like to know the Junction- Case Thermal Resistance and Max Junction Temperature for S25FL256SAGMFI001. Thanks, Prathik Show More
peakjohn
Nor Flash
Dear all:      It seems some errors in S79FS01GS Datasheet      In chapter "Ordering Information" , what it described is S25FS series      In Packages... Show More
vijayks
Nor Flash
Hi,        I was facing the problem in writing and reading the data into the Flash memory of S25HL512T in QSPI mode. I have the Flash to operate in QS... Show More
Grace
Nor Flash
Hello Team, Could you please share maximum junction temperature (Tjmax) of S25FL064LABNFM040 for all modes?  Regards, Grace Show More
NL
Nor Flash
We are planning on using S25FL256SAGNFI003 in a new PCB design we are doing.  However, I was not able to find if the exposed pad should be connected e... Show More
JJ_II
Nor Flash
Since AMD Flash memory spun off to Spansion and then to Cypress who is part of Infineon I am coming here with a question about how production location... Show More
Board Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.
Top liked authors