Nor Flash

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
LuisDuarte
Nor Flash
Hello, good morning.I got some doubts regarding the S70FL01GSAGMFI010 flash memoryAs it works with SPI, I would like to know if it is possible to use ... Show More
Vivian0114
Nor Flash
We bought the part  S25FL512SAGMFIR10, the date code is 19+ , but the marking is different from what data sheet said. Is there anyone who can help to ... Show More
Daniel-Gull
Nor Flash
Hi Bushra I registered for the Semper Access Program (AP) on January 11, but still do not have full access to the datasheets for S25HL512TDPNHI010. In... Show More
NXTY_Nagata
Nor Flash

Hi,

Can you provide IBIS model for S29GL256P90TFIR20?

Regards,
Nagata

l0p0c
Nor Flash
Stm32h743 is connected via FMC s29gl064s,and cubeide configed. As shown below:   RCC configured as below: Read flash ID: sts = HAL_NOR_Read_ID(&hnor... Show More
Shivam_Shah
Nor Flash
Hello, I have replaced my Winbond flash w25q256jv with S25FL256SAGNFI010. What are the major electrical points I have to take care of while designing ... Show More
GlenLee
Nor Flash
Sir,   Do we have sample code to let customer know how to exit safe-mode of Semper flash ?   Thanks.   Glen Show More
l0p0c
Nor Flash
The FLASH detailed model is S29GL064S70TFI070.   Is the flash ID correct??? Read flash ID: sts = HAL_NOR_Read_ID(&hnor1, &id);printf("sts1 = %d\n", st... Show More
Shivam_Shah
Nor Flash
hello, I want to replace my Winbond flash w25q256jv with S25FL256SAGNFI010.which changes I have to do to configure flash or else in the program and in... Show More
User21260
Nor Flash
Hi,I am using flash memory part S25FL064L in my design.I wanted to know the "Write cycle time" to Write 1 Byte data into this memory.In the datasheet,... Show More
Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.
Top liked authors