Nor Flash Forum Discussions
text.format{('custom.tabs.no.results')}
We are upgrading from the S70FL01GSAGMFI011 and we would prefer a drop in replacement. We care more about the radiation hardening than the extended temperature range.
Show LessHello,
I was hoping to load default values into the memory array, CFI field and protection bits for the S29GL512S12DHE010 for the VHDL simuation model for the S29GL512S. How do I do this? The user manual leaves a lot to be desired and I dont know how to do it. It would be great if one could be created for me. It looks like if I make the UserPreload false, it defaults everything to undefined (U) and I would think that would force me to issue an erase command then send a write command. The test bench calls out these files as constants but I dont see where these files are at all for a different flash part. All I want to do is send write to buffer, and word program commands. I may also want to read commands so having a template of sort that I can modify would be a great help. Unfortunally the provided simulation model to my knowledge doesn't address this at least in a clear, easy to understand way. Essentially I want my simulation to have FFFF written everywhere to start.
Thanks, Dan
Note: I asked this in the Community information topic area by mistake.
Show LessHello Team,
We are planning to use S25FL256LAGMFV000 NOR Flash in one of our design. But over digikey it is showing as "NO WARRANTY".
Is this correct? Please share information for the same.
Regards,
Vaidehi
Show LessWhat is the difference between S29PL032J70BFI120 and S29PL032J70BFI070?
S29PL032J70BFI120 is reported to be Obsolete with NO replacement per PTN181204 or PTN181204A.
A quick glance at old Spansion datasheets appears to show Spansion's S29PL032J70BFI120 is equivalent to Cypress' S29PL032J70BFI070 other than the Max Sector Erase Time increased from 2 seconds to 5 seconds. The typical Sector Erase Time for both parts is listed as 0.5 seconds.
The web page for S29PL032J70BFI120 points to data sheet revision F that lists S29PL032J70BFI070 but does not include S29PL032J70BFI120.
Valid suffixes in data sheet revision F appear to be 04x through 10x.
The previous Spansion S29PLxxxJ datasheet shows options 00x through 03x and 12x through 13x.
It appears the mapping is:
From 00x to 04x (3.0V VIO, 80-ball 8 x 11 mm FBGA (VBG080))
From 01x to 05x (1.8V VIO, 80-ball 8 x 11 mm FBGA (VBG080))
From 02x to 06x (3.0V VIO, 64-ball 8 x 11.6 mm FBGA (VBH064))
Suffix 03x was deprecated (1.8V VIO, 64-ball 8 x 11.6 mm FBGA (VBH064))
From 12x to 07x (3.0V VIO, 48-ball 8 x 6 mm FBGA (VBK048))
From 13x to 10x (3.0V VIO, 56-ball 7 x 9 mm FBGA (TBD))
Suffix 08x and 09x were added (3.0 and 1.8 VIO, 56-pin 20 x 14 mm TSOP (TS056))
Greg
Show LessHello,
I was hoping to load default values into the memory array, CFI field and protection bits for the S29GL512S12DHE010 for the VHDL simuation model for the S29GL512S. How do I do this? The user manual leaves a lot to be desired and I dont know how to do it. It would be great if one could be created for me. It looks like if I make the UserPreload false, it defaults everything to undefined (U) and I would think that would force me to issue an erase command then send a write command. The test bench calls out these files as constants but I dont see where these files are at all for a different flash part. All I want to do is send write to buffer, and word program commands. I may also want to read commands so having a template of sort that I can modify would be a great help. Unfortunally the provided simulation model to my knowledge doesn't address this at least in a clear, easy to understand way.
Thanks, Dan
Show LessHello,
I am going to use NOR flash part S25FL512SAGBHVA10 in my design with VCC= 3.3V and VIO=1.8V.
Please provide the maximum current consumption in VIO power supply.
Thanks in advance,
Sakthi
Show Less