Nor Flash Forum Discussions
I am working with a NOR Flash part that uses Infineon dye and have experienced a single bit error. I believe it to be pseudo Single Bit Charge Loss and found Infineon's application note for high reliability programming using a second "Program" step before verifying. Using Windriver Workbench as a flash driver, is it as simple as pressing the "Program" button twice?
Thanks,
Aaron
Show LessMy name is Justin and I’m interested in identifying microelectronic supply chains for parts of interest. In support of this effort, I need to identify physical locations (address) of products that they produce (design, fabrication sites, assembly sites, distribution and final test sites). Your assistance would be greatly appreciated in identifying the manufacturing (design, fabrication, assembly, distribution and final test) physical address sites of the following products:
Am29F160DT75EF
MBM29F160TE-90TN-E1
Thank you for your time,
Justin
Show Lesshi,
pls assist to provide IBIS model for S29GL01GS12DHE023
Thanks.
BC
Hello All,
In Linux Kernel-4.9.65, tried the S25HS512T flash chip.
Able to read the Manufacturer Id, Device Id MSB and device id LSB.
Able to perform the Write Status Register1 and read the status register 1.
But Write operation is not working. Here, SPI clock is 38.5 MHz
Please provide your inputs.
-Thanks.
Show Less
How do I connect the exposed pad for WSON packages used with S25FL064LABNFI011 Flash? Should it connected to ground?
Hello
I want to see if 1.8v io serial nor flash memory is available and what is the part number? Any leadte information for the same.
This is for space application.
Amar
Show LessDear supporters,
How do I connect to the MCU when S29GLxxx P is set in byte mode access?
My understanding is as follows, is it correct?
MCU - S29GLxx
A22 - A21
A21 - A20
A20 - A19
… …
A3 - A2
A2 - A1
A1 - A0
A0 - DQ15/A-1
Regards,
Nagata.
Hi Team,
Please assist me with an alternate for this part S29CD032J0MQFM010.
What are the estimated cost of CYRS16B512 and full part number parameters?
In relation to this application note, does this affect all NOR Flash specifically S29JL064J?
If a pSBCL event occurs, does it typically effect more than a single bit?
Is an erase cycle performed on the front end of a program cycle? For example is a whole page erased and then rewritten even if only programming a single byte? As a follow up, what is the smallest erasable section of the memory when performing a program instruction?
The application note states that a true SBCL defect can be determined and repeated. For that event what is the worst case voltage and temperature to exacerbate the defected cell?
Show Less