Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Nor Flash Forum Discussions

Sort by:
camino
Nor Flash

How can I get the low level driver of  SEMPER NOR flash products ?

I can not find them in website.

MAO
Nor Flash
I am wondering if it is OK to set the minimum time from the negation of chip selection to the assertion of chip selection at 20ns for read instruction... Show More
jpaolino
Nor Flash
Hello, Looking at the S25HS Family of QSPI, I see the Output Valid (Tv) for the HS-T ranges from 2-6nS.  Is the max value entirely dependent on capaci... Show More
anuragps
Nor Flash
Hi, I am using  SPI Serial Flash Memory, 512Mbit, SO16 package in one of my design. I am finding many chips getting faulty in 5 to 6 months of operati... Show More
C_T_T
Nor Flash
I am trying to change the "Infineon Endurance Flex architecture Selection Register" of S25HL512. for example, After doing WRENB_0_0(0x06), 0x71,0x00,0... Show More
cyldz
Nor Flash
Hello, I am using S25FS512SAGNFI011 Nor Flash for the FPGA Arria 10 configuration. I generated .jic file from .sof file as described in the document A... Show More
MAO
Nor Flash

Please tell me about θjc or Ψjt and θjb or Ψjb of Infineon S29AL016J70TFI010.

Barath3
Nor Flash

What is the weight of S25FL512SAGMFI011?

MAO
Nor Flash

S25FL128SAGMFI000
Do you have experience with the above model numbers operating at clock frequencies below 300 kHz?

MAO
Nor Flash
The S29AL008J70BFI010 datasheet lists the sector trace time as "10s",The S29AL008J70BFI010 datasheet lists a maximum sector trace time of 10s.I unders... Show More
Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.