Nor Flash Forum Discussions
Hi,
What is the allowable junction temperature range for S29AL008J70TFI010?
Best Regards,
Kumada
Hi,
in our application we need to be able to do erasing in short time slices as we are on a very tight power budget. We couldn't find the answer to our question from the datasheet or from the forums.
My questions are:
1. What is the recommended minimum time between Erase-Resume command and Erase-Suspend command?
2. What is the recommended minimum time between Erase-Suspend command and Erase-Resume command?
Thank you in advance!
Show Less
Hello,
I designed a board with a zynq and S25FL128SAGBHI200 memory for boot.
The memory seems to be recognized sporadically and it is impossible for me to program it. I would like to check signal integrity of the memory bus by simulation tool. For this, I would like to have the ibis model.
Is it possible to get the IBIS simulation model for the reference S25FL128SAGBHI200 .
Thank you for your help.
HyperBus recognizes that Octal and InterFace are standardized, but are there any specific differences?
Firstly, hardware is connected and the programmed is erased with Jflash, then, Jflash fails to connect with power cut and restart but succeeds to connect if firstly connected with RVDS. Hardware works in a normal way.
How can I solve this issue?
Hi,
Can you tell me about the VCC current during power-on for S29GL032N90TFI030?
I checked the datasheet but could not find it.
Best Regards,
Kumada
Show LessHello,
In S25FL256 datasheet, speed option DP is 66 MHz DDR.
Does it mean that this memory only can work in DDR mode?
Can it work in SDR mode?
Many thanks and regards
Show LessAccording to the following post, the S70FS01GS must be configured before use:
But I used the device without configuring the CR1NV and CR3NV registers. Does that mean that the device is now unusable?
I saw in the data sheet that these registers cannot be changed if the IC has been erased/written.
Will the IC not work in the default state (both registers at 0)? Is that an invalid configuration from factory?
Show LessHi,
Under an environment of 100°C,
does the Data Retention Time Minimum Time=20years (10K Program/Erase Cycles) described in the datasheet?
Best Regards,
Kumada
Show Less