Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Nor Flash Forum Discussions

croura
Nor Flash
I am trying to send the command to erase multiple sectors but only the first sector is being erased. I am sending  Address Data 0x555    0x00AA 0x2AA ... Show More
lukasfrank
Nor Flash
Hi Dear Authorized,   I am trying to use HyperFLASH over FlexSPI Interface over HyperBUS and some errors occured during test on my custom board which ... Show More
YuMa_1534086
Nor Flash
Hello Infineon.   Please confirm below questions. Device is S29GL256S10TFIV10.     Q1) Are there any conditions or timing under which this flash will ... Show More
camino
Nor Flash
Hi, We plan to migrate to S29G128P to S29128S. The data bus width is x16. Pin 53 (BTYE#) in TSOP should be connected to VIH in S29G128P. In case repl... Show More
ThomasDoering
Nor Flash
Hi everyone, in our embedded device we are using the very old release of the SpansionFS v1.0 (including NAND-LLD and FTL).Unfortunately we have some s... Show More
Cris
Nor Flash
Hello, for an application we are developing, I need to know the Flash identification (vendor code and device code) in order to access the flash proper... Show More
RamaKrishnan1
Nor Flash

Kindly provide Junction Temperature and FIT/MTBF data for S70FL01GSDSMFV013 and S25FL128SAGNFV010

zhaohuwen
Nor Flash

我们使用英飞凌的IC(p/n: S25FL064LABMFV000)进入QPI 模式被锁,无法解锁。

jabreen
Nor Flash
For the S29GL01GT flash, is setup & hold timing measured relative to CE# being asserted? For example, suppose we're doing a CE#-controlled write.  If ... Show More
Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.