Nor Flash Forum Discussions
Hello
The customer is operating the Write to Buffer at 128 words, but writing can not be completed.
When writing to buffer 64 words once was successful, but writing to buffer (128words) once
fails.It will freeze during writing and the writing will not be completed.
We confirmed that Write to Buffer (128 words) will succeed when SA's address is round number such as 7D0000h, 7D0100h, 7D0200h, 7D0300h etc. However when SA addresses are
7D0020h, 7D0120h, 7D0220h. . .128 words writing did not succeed
In details, after operating “Program Buffer to Flash” command, 0x0098 is set to RD of “Status
Register Read” command.
Are there restrictions on the difference of SA's address? Or are there any other reasons mentioned
above?
Best Regards
Arai
Show Less
Hello,
I am working on S25FL164K0XMFI011 NOR flash with SPI interface.
What are recommendations for SPI communication at noisy environment?
Typically it is good practice to add series resistances to clock and signal lines. But what is the best value?
Is it allowed to place additionally capacitor directly connected to MISO (e.g. 100pF).
Can pull-up/pull-down resistors be helpful?@
Show LessHi Krishna,
Please advise why the set top box cannot boot after we used S29GL128P11FFIS40 to replace S29GL128P10FFIS10. The both of the parameter is very similar after compared with the spec, is it possible to adjust the software to make it working?
Jennifer Zuo
Show Lessコマンド06h にてWREN発行後、コマンド 05hでStatus Register 1のWELを 見にいった場合、即座にWEL=1という状態になりますでしょうか? この場合(06h発行後、Status Register 1のWELが”1”になるまで)のmax時間を ご教授いただくことは可能でしょうか?
Show LessHello. Could someone suggest me which of current Cypress products can be used as a replacement for obsolete AM29LV641DL-90REI flash memory.
Thank you in advance.
Best Regards,
Damir Tadic
Show LessCustomer is considering their board design for below two parts now.
#1.S25FS512SDSBHM210
#2.S70FS01GSDSBHM210
Q1. I can see Theta JA of FAB024 package as 39degC/W in S25FS512S datasheet,but I can not see it in S70FS01GS datasheet.
Let me know the Theta JA of FAB024 for 70FS01GS.
Q2.Does AN201006 correspond above two parts?
http://www.cypress.com/file/210756/download
( I would like to know refence model of the theta JA sach as JESD15 and Ta spec etc.)
Q3.Do you have specs of Theta JB (junction to board) and Theta JC(junction to case) for above two parts?
Ecpected due date : 17th.Oct.
Thank you & Regards,
Masaya
Show LessHello,
Micron W29DW Flash has reset command (F0) of 1-Cycle and 3-cycle.
1-cycle:
Adder | Data
x | F0
3-cycle:
555 | AA
2AA | 55
x | F0
Now, customers are considering changing from Micron to Cypress's S29GL128S.
According to the data sheet, GL-S supports only 1-cycle reset command (F0).
If 3-cycle reset command is issued, will GL-S Flash execute reset?
Or is this command ignored?
Best Regards,
Naoaki Morimoto
Show LessThe internal data changes during we using S29JL032J70TFI020, can you give us advice why the situation would occurred?
Part#: S29JL032J70TFI020
Period of use: about 18 months
Failure: data 00 turns to 01 automatically
Show LessThe minimum erasesize of this chip is a Sector, wich for this chip is 4KB throughout the whole chip.
So I only need 4KB Buffers / Caches instead of 4KB + 64KB for higher regions.
Is my understanding of the datasheet correct?
Thanks !
- Dominik
Show Less