Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

Nor Flash Forum Discussions

Sort by:
SuSh_1535366
Nor Flash
S29GL064N90TFI070のEOLに伴い、S29GL064S70TFI070での置き換えを検討しています。マイグレーションガイドAN98586では、64Mbitは除外すると記載されています。上記組み合わせでの置き換えは可能なのでしょうか?また、64Mbitと128Mbit以上の違いはどこにあ... Show More
JUTA_2823561
Nor Flash
What are the θJC (Theta Jc) and Tjmax values of S29GL01GS11DHV020?S29GL01GS11DHV020 Theta Jc : ? C/W Tjmax    : ? C Show More
JUTA_2823561
Nor Flash
What is the initial value when Nor FLASH (S29AL008J70TFI020) is shipped? (All = 0x00, FF, other) Show More
xiaowei_li_3787
Nor Flash
HiI am using the flash chips of CYPRESS,S25FL128SAGNFI000, but I have 2 questions that i don't understand..1, I want to configurate the SR1 and CR1, s... Show More
toyac_1469256
Nor Flash
S70GL02GSは2Chip搭載の製品になりますが、一方のChipへErase or Write 動作実行中に、他方のChipにてRead動作は行えますか?内部動作中にはStatus dataが出力されると思いますが、CE#やアドレス指定にて、内部動作中でない方のChipを選択すれば、保証はしない... Show More
JoBa_2147096
Nor Flash
Hi,I apologize if I post this question twice.  I am not sure if my initial post was captured.I am looking for Cypress cross to the MT28EW01GABA1HJS-0S... Show More
DaWi_3430881
Nor Flash
Hello memory experts,   I have a custom system that uses two nor S70GL02GS12 devices in parallel to create a 32-bit data bus which is connected to an ... Show More
ToKo_1330256
Nor Flash
ご担当者様以下、御教示頂けますと助かります。・フロー半田(リフローではなく)は可能ですか? 可能な場合の条件。・コーティング 可否、可能が場合の条件。・水洗浄は可能ですか?宜しくお願い致します。 Show More
JoBa_2147096
Nor Flash
Hi, I need a cross for the I need a cross for MX29LV040CQI-70G.  I can't find this part number on the on line cross reference sheet.thanks,John Show More
Anonymous
Nor Flash
Hello,I would like to bulk erase the complete memory ( i.e. both the devices FS512S).Since I am pretty new to this Flash memory , I would like to know... Show More
Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.