Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

Nor Flash Forum Discussions

Sort by:
xiaowei_li_3787
Nor Flash
Hi,I am using the flash chip of CYPRESS, S25FL128SAGMFI000,  but I have some questions that I don't understand .After power up, I did the RDSR1 comman... Show More
user_60784
Nor Flash

how to program Advanced Sector Protection for S29GL128P, need examples

ShYa_3490236
Nor Flash
Hi, I am looking for counterparts list of current Micron parts.I found the below link but part number does not match completely. So, please let me kno... Show More
siasc_4048026
Nor Flash
Hello Cypress community,I want to use S25FL256SAGMFI003 SOIC-16, with 1.8V procsessor. I had a doubt about 1.8V working because I faced with this sent... Show More
NaMo_1534561
Nor Flash
Hello,NOR Flash with automatic ECC function will generate valid ECC code when issuing the Write Buffer Programming command.On the other hand, when exe... Show More
xiaowei_li_3787
Nor Flash
HiI am using the flash chip of CYPRESS,S25FL128SAGNFI000, but I have some questions that i don't understand when I do the simulation.I am doing the si... Show More
toyac_1469256
Nor Flash
Although the definition of the Typ value and the Max value is stated in Note 1, is it OK to say that it approaches the Typ value at 100,000 time P / E... Show More
toyac_1469256
Nor Flash
Is the content below wrong?If you make a mistake, will you fix it?■ Page 23: PL 127 J Sector ArchitectureAlthough it is described up to SA111, it is S... Show More
jusac_3935691
Nor Flash
hi.I found information about NOR Flash in the following document.http://www.cypress.com/file/275051/downloadP. 23  3.3.5 NOR FlashAnd I want to use th... Show More
NaMo_1534561
Nor Flash
Hello,According to the data sheet of S29GL-T, there is a method of status check by polling using DQ3 when executing the sector erase command.Is this a... Show More
Forum Information

Nor Flash

The NOR Flash Memory forum discusses critical safety features for automotive and industrial systems, and Semper NOR Flash Memory with ASIL-B compliant and ASIL-D-ready.