Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
keni_4440091
Level 7
Level 7
500 replies posted 100 solutions authored 50 solutions authored

Dear supporter

Infineon TC3 family has Queued SPI function which can achieve serial interface.

Please let me know if Cypress Quad SPI NOR Flash memory would be suitable on communication with this function in the follwing clock rate.

Please refer to the following spec Page-2.

https://www.cypress.com/file/209446/download

pastedImage_0.png

And regarding this definition, "MBps" means mega Bit per sec ? Or mega Byte per sec ?

The following definition shows current consumption with several reading speeds in spec Page-2.

Is the high speed reading value in the following table depend on MCU baud rate setting ?

pastedImage_0.png

Regards,

Nino

0 Likes
1 Solution

The SPI clock frequency depends on the MCU and should not exceed the maximum frequency specified in the datasheet.

View solution in original post

0 Likes
8 Replies
ShupingZ_76
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

"MBps" means mega Byte per sec.

Also, could you please provide the OPN?

0 Likes

What is OPN ?

0 Likes
ShupingZ_76
Employee
Employee
50 solutions authored 25 solutions authored 10 solutions authored

OPN means ordering part number.

0 Likes

No order parts # for this customer, because just looking the spec as "S25FL256L / S25FL128L".

Please repy the bottom question. Thanks.

0 Likes

The SPI clock frequency depends on the MCU and should not exceed the maximum frequency specified in the datasheet.

0 Likes

Let me ask an addition question on this topic.

There are two difinition in spec as "READ w/ 50MHz" and "High speed READ w/ 133MHz".

How customer can set the speed for reading w/ above spec ?

Let me know merit and demerit for normal reading and high speed reading on customer usage.

Regards,

Nino

0 Likes

Please check Section 8. Command in the datasheet​ :

pastedImage_0.png

There is a "READ" command and a "FAST_READ" command.

"READ" command supports up to 50MHz, while "FAST_READ" command supports up to 133MHz.

0 Likes

Thanks.

Regards,

Nino

0 Likes