- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Ive been trying to source the S25FL128SAGNFI000, which we successfully integrated into a past build, but the broker working for us only found S25FL128SAGNFI010 available. Are these compatible with one another? Could you please detail the major differences between them so that I can submit this information to my design engineers, electrical engineers, and software engineers? We really need this memory, but I don't want to mistakenly purchase something which is not going to work. At a high level, most of the specs of these two units are almost mirror images of one another, but I suspect there had to be a reason for the model number change. Thank you for your help.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Scott,
Thank you for contacting Cypress Technical Support, an Infineon Technologies Company. Please see below
S25FL128SAGNFI000
S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory
128 - 128 Mb
S - 65 nm MirrorBit Process Technology
AG - 133 MHz
N - 8-contact WSON 6 x 8 mm package
F - Halogen-Free, Lead (Pb)-free
I - Industrial (-40°C to + 85°C)
0 - EHPLC, SO/WSON footprint
0 - Uniform 64-KB sectors
0 - Tray
S25FL128SAGNFI010
S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory
128 - 128 Mb
S - 65 nm MirrorBit Process Technology
AG - 133 MHz
N - 8-contact WSON 6 x 8 mm package
F - Halogen-Free, Lead (Pb)-free
I - Industrial (-40°C to + 85°C)
0 - EHPLC, SO/WSON footprint
1 - Uniform 256-KB sectors
0 - Tray
Difference is sector type.
Please refer to datasheet for more information.
https://www.cypress.com/file/448601/download
Thank you
Regards,
Bushra