What is the difference between the S25FL128SAGNFI000 and the S25FL128SAGNFI010

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Scott1
Level 1
Level 1
First question asked Welcome!

Ive been trying to source the S25FL128SAGNFI000, which we successfully integrated into a past build, but the broker working for us only found S25FL128SAGNFI010 available.  Are these compatible with one another?  Could you please detail the major differences between them so that I can submit this information to my design engineers, electrical engineers, and software engineers?  We really need this memory, but I don't want to mistakenly purchase something which is not going to work.  At a high level, most of the specs of these two units are almost mirror images of one another, but I suspect there had to be a reason for the model number change.  Thank you for your help.

0 Likes
1 Solution
BushraH_91
Moderator
Moderator
Moderator
750 replies posted 50 likes received 250 solutions authored

Hello Scott,

Thank you for contacting Cypress Technical Support, an Infineon Technologies Company. Please see below

S25FL128SAGNFI000

S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory

128 - 128 Mb

S - 65 nm MirrorBit Process Technology

AG - 133 MHz

N - 8-contact WSON 6 x 8 mm package

F - Halogen-Free, Lead (Pb)-free

I - Industrial (-40°C to + 85°C)

0 - EHPLC, SO/WSON footprint

0 - Uniform 64-KB sectors

0 -  Tray 

 

S25FL128SAGNFI010

S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory

128 - 128 Mb

S - 65 nm MirrorBit Process Technology

AG - 133 MHz

N - 8-contact WSON 6 x 8 mm package

F - Halogen-Free, Lead (Pb)-free

I - Industrial (-40°C to + 85°C)

0 - EHPLC, SO/WSON footprint

1 - Uniform 256-KB sectors

0 -  Tray 

Difference is sector type. 

Please refer to datasheet for more information.

https://www.cypress.com/file/448601/download

 

Thank you

Regards,

Bushra

View solution in original post

0 Likes
1 Reply
BushraH_91
Moderator
Moderator
Moderator
750 replies posted 50 likes received 250 solutions authored

Hello Scott,

Thank you for contacting Cypress Technical Support, an Infineon Technologies Company. Please see below

S25FL128SAGNFI000

S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory

128 - 128 Mb

S - 65 nm MirrorBit Process Technology

AG - 133 MHz

N - 8-contact WSON 6 x 8 mm package

F - Halogen-Free, Lead (Pb)-free

I - Industrial (-40°C to + 85°C)

0 - EHPLC, SO/WSON footprint

0 - Uniform 64-KB sectors

0 -  Tray 

 

S25FL128SAGNFI010

S25FL - Cypress Memory 3.0 Volt-Only, Serial Peripheral Interface (SPI) Flash Memory

128 - 128 Mb

S - 65 nm MirrorBit Process Technology

AG - 133 MHz

N - 8-contact WSON 6 x 8 mm package

F - Halogen-Free, Lead (Pb)-free

I - Industrial (-40°C to + 85°C)

0 - EHPLC, SO/WSON footprint

1 - Uniform 256-KB sectors

0 -  Tray 

Difference is sector type. 

Please refer to datasheet for more information.

https://www.cypress.com/file/448601/download

 

Thank you

Regards,

Bushra

0 Likes