Hi Team,
Please let me know Tjmax for S25FL256LAGNFB010.
I understand that Tj@Pdmax is 108.888℃ for S25FL256LAGNFB010.
・Tj@Pdmax = ( 18 x 0.216 ) + 105 = 108.888 (℃).
At this time, I am required Tjmax for S25FL256LAGNFB010, so please advise this.
Or, please provide Flash Memory version of AN4017.
Thanks and regards,
Solved! Go to Solution.
Hello,
Please see my comment below:
・Absolute Maximum Junction temperature with the Power Applied = 125℃.(do not operate FLASH at 125C; operation is not guaranteed).
Answer: Yes your understanding is correct.
・Maximum Operating junction temperature = 108.9℃ (based at max ambient of +105C).
Answer: Based on my calculation, max operating junction temperature at Pd max should be as follow.
- theta ja = 18 degrees C/W
- max current = 50 mA
- max voltage = 3.6 V
- Pd max = 180 mW
- max. Operating junct. temp. = (106.8 C (based at max ambient of +105C)
Thanks,
Nada