- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
S70FL01GSAGMFI011 have a pin VIO/RFU, but the datasheet said:
Note that the Versatile I/O (VIO) power supply (pin 14 on the 16-pin SO package and ball E4 on the 5x5 BGA package) is not
supported, and pin 14 and ball E4 are RFU (Reserved for Future Use) in the standard configuration of the S70FL01GS device.
Contact your local sales office to confirm availability with the VIO feature enabled.
If CYP have this product with VIO function? -- I can power 3.3V or 1.8V to VIO.
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Yong,
The part S70FL01GSAGMFI011 does not support VIO = 1.8V. If you are interested in 1.8V I/O, we recommend you the part S70FS01GS which is available and supports 1.8V Core and IO voltage.
Please refer the datasheet of S70FS01GS from the link given below :
http://www.cypress.com/file/215911/download
Thanks,
Krishna.