Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Nor Flash Forum Discussions

YoBa_2719251
Level 1
Level 1

Hi

S70FL01GSAGMFI011 have a pin VIO/RFU, but the datasheet said:

Note that the Versatile I/O (VIO) power supply (pin 14 on the 16-pin SO package and ball E4 on the 5x5 BGA package) is not

supported, and pin 14 and ball E4 are RFU (Reserved for Future Use) in the standard configuration of the S70FL01GS device.

Contact your local sales office to confirm availability with the VIO feature enabled.

  If CYP have this product with VIO function? -- I can power 3.3V or 1.8V to VIO.

0 Likes
1 Solution
Anonymous
Not applicable

Hi Yong,

The  part S70FL01GSAGMFI011 does not support VIO = 1.8V.  If you are interested in  1.8V I/O, we recommend you the part S70FS01GS which is available and supports 1.8V Core and IO voltage.

Please refer the datasheet  of S70FS01GS from the link given below :

http://www.cypress.com/file/215911/download

Thanks,

Krishna.

View solution in original post

0 Likes
3 Replies
Anonymous
Not applicable

Hi,

The device S70FL01GSAGMFI011  is a standard configuration part and does not support VIO feature as mentioned in the datasheet.

In this case the pin is RFU.

If you need a device with VIO feature please contact sales office nearer to your region.

The device with VIO feature will support I/O Supply Voltage from 1.65V to 3.6V

Thanks,

Krishna.

0 Likes

Hi:

    Pls help to confirm : S70FL01GSAGMFI011 don't support VIO feature,  If  S70FL01GSAGMFI011 will support I/O Supply Voltage from 1.65V to 3.6V ?

0 Likes
Anonymous
Not applicable

Hi Yong,

The  part S70FL01GSAGMFI011 does not support VIO = 1.8V.  If you are interested in  1.8V I/O, we recommend you the part S70FS01GS which is available and supports 1.8V Core and IO voltage.

Please refer the datasheet  of S70FS01GS from the link given below :

http://www.cypress.com/file/215911/download

Thanks,

Krishna.

0 Likes